Skip to main content

Kollmorgen Support Network

AKD PDMM

A component of the Kollmorgen Automation Suite, the AKD PDMM™ Drive Resident Controller combines an integrated AKD servo drive with an embedded motion controller that can control up to 64 axes, and the full automation capability of Kollmorgen Automation Suite™ in a single, compact package.

Current Drive Firmware Version1.25.00.000
Current Runtime Firmware Version4.05 R1
Firmware Release DateMay 2026
Firmware History & DownloadsKAS Associated Firmware by Release
Current Hardware RevisionEB
Part Number SchemeOpen the PDF
KAS-IDE Compatibilityv4.05 R1 and later
Current KAS-IDE Versionv4.05 R1
Release DateMay 2026
ModelProcessor
AKD-M0xxxx-MCEC800 MHz single-core
AKD-M0xxxx-M1EC1.2 GHz single-core

Interfaces

Digital/analog I/OsMultiFieldbusPosition output (encoder emulation)Software interfacesMultiFeedback
  • 1  programmable analog input
  • 1  programmable analog output
  • 13 programmable digital inputs
  • 6 programmable digital outputs
  • 1 Enable input
  • 1 STO input 
  • Emulation incremental encoder  
  • Ethernet TCP/IP Service channel
  • Modbus TCP Service channel
  • HTTP requests
  • UDP
  • ProfiNet
  • EtherNet/IP
  • SSH

See Protocols Supported by AKD Drives for more products

 

Grounding and Shielding Landing Page (Prevent Noise Issues) English
Ann Pater
AKD2G and KAS Functional Safety Landing Page  English
C Wontrop
KAS v3.07 is now available!! English
dusty.…
SafePLC2 Project integrated in KAS IDE software English
Joe Parks
What is a Subnet Mask? English
jcoleman02 jcoleman02
Resolving Servo Feedback Choices English
kenny.…
KAS Stepper Control with AKT2G slices English
Joe Parks
Coupler Sizing - AKT2G Remote IO English
C Wontrop
Configuring BBH SCU with AKD2G SRA parameters English
jeeva
How do I restore communication with the drive if I have lost communication and the IP address in the drive is 0.0.0.0.?

First, check the LED on the RJ45 connector. If the LED is not illuminated, then no communication with the drive is possible. Possible causes for loss of communication with the drive include:

  • The network cable is disconnected.
  • A wiring problem exists between the drive and the network switch/hub.
  • The switch/hub is not powered.

If the LED is lit and the IP address on the drive is 0.0.0.0, then the most likely problem is that the drive hardware has not detected a valid link.

During the installation, a dialog box saying “Please wait while the installer finishes determining your disk space requirements” appears and never disappears. How do I remove this box?

This problem is related to the MSI installer. You can resolve it as follows:

  1. Cancel the installation.
  2. Make sure that you have enough disk space on your hard disk (~500MB) to allow Windows .NET update if necessary. If you do not have enough disk space, then make additional space for the installation.
  3. Relaunch the installer (you may need to try this several times, the problem is random).