Skip to main content

The Precision Challenge in Automotive Logistics

Automotive manufacturing runs on precision. Every component must arrive at the right place, at the right time. With just-in-time production, even minor delays can disrupt the entire line. Manual handling, while essential in many operations, can sometimes create challenges when large volumes, tight schedules, or heavy and high value parts are involved.

Automation plays a key role in solving these challenges. AGVs and AMRs ensure consistent material flow, reduce human error, and keep production moving without interruption. By automating repetitive transport tasks, manufacturers gain better control over timing and accuracy, while freeing skilled workers for higher-value activities. 

car chasis
car manufacturing automation

ROI and Efficiency – Proven Results

Automation isn’t just about technology—it’s about measurable gains. With AGV fleets, manufacturers see: 

  • Optimized Routes: Intelligent software calculates the most efficient paths, reducing travel time and bottlenecks.
  • Reduced Downtime: Opportunity charging and smart scheduling keep vehicles running around the clock.
  • Increased Capacity: Automated systems handle more transports per hour than manual operations.

Toyota Material handling & Gundlach Automotive: High-Volume Precision

At Gundlach Automotive, 12 Toyota Material Handling AGVs powered by Kollmorgen manage 150 transports per hour, handling 40,000 pallet spaces with a 2,500 kg load capacity and lifts up to 11 meters. Integrated with 16 RadioShuttles and guided by Kollmorgen’s fleet manager, the system ensures deep pallet storage and efficient retrieval—keeping high-volume automotive logistics running smoothly. 

Watch Video Visit Website

Toyota material handling
ek robotics & Aston Margin car manufacturing

Ek Robotics & Aston Martin: Precision in Motion

At Aston Martin, each vehicle undergoes a 200-hour handcrafted build, supported by advanced automation. Customized high-reach AGVs from ek robotics, powered by Kollmorgen’s NDC Solutions, transport body parts and chassis with laser navigation, steer drive, and a 6-meter lift capability—ensuring precision and productivity in a premium manufacturing environment. 

Watch Video Visit Website

Dematic & Bridgestone: Smart Stillage Handling

At Bridgestone’s Australian warehouse, Dematic deployed counterbalance AGVs powered by Kollmorgen’s NDC Solutions to automate stillage handling for car and truck tires. With a 1,500 kg load capacity, 4-meter lift height, and block-stacking capability, the system streamlines stacking tasks and uses opportunity charging to keep operations running efficiently—freeing forklifts for critical work and boosting productivity.

Watch Video Visit Website

Dematic youtube video

Let’s build the future together

Whether you’re an AGV/AMR provider or integrator, Kollmorgen NDC Solutions give you the edge to succeed – today and tomorrow.

Explore NDC Solutions Contact Our Experts

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.