Skip to main content

Kollmorgen Support Network

AKD-C/N

The AKD-C Power Supply and AKD-N drives lie at the core of a decentralized drive system. Up to 16 AKD-N drives can be connected to one AKD-C central power supply. Hybrid cables are used to connect the AKD-C to the drives and to daisy-chain the drives. For more specific information about the individual components, see the AKD-C and AKD-N topics.

Current Firmware Version 1.20.00.001
Firmware Release Date December 2020
Current Hardware Revision (AKD-N) B
Current Hardware Revision (AKD-C) A
Hardware Release Date 01/01/2014
Part Number Scheme AKD-N (PDF)
AKD-C (PDF)
See the WorkBench article for details about the software used to configure and manage the drives.
Components
AKD-C Central Power Supply
AKD-N Decentralized Servo Drive

Blue Boxes: All components in the blue box are products delivered by Kollmorgen. For detailed information click to the product or use the table below for navigation.
Gray Boxes: Elements in the gray area are components which have to be added by the machine builder.

image

AKD-C AKD-C Power Supply
AKD-N AKD-N Drive
AKD-CN-Coupling Connector interface for cabinet wall (in process)
AKD-M AKD PDMM Drive
AKM AKM Motor
AKMH AKMH Motor
AKI Operating Console
AKT KAS Input and Output Terminals
BAR/BAS/BAFP Brake Resistor
Cx Cables Configured CC/CM/CF cables for connection of the components, refer to the cable part number scheme
DDL Linear motors (on request)
ENCP Ethernet cables
Gearhead Micron Gearheads
Heatsink Kit optional accessory for AKD-N
KAS-IDE KAS System Setup Tool
KBM KBM Motor
KCM KCM Capacitor Module
Redi Mount Adapters to mount Micron Gearheads to AKM motors
Workbench AKD Setup Tool
Trade Compliance English 21 Feb 2023
Bethany Seymour Bethany…
KAS v3.07 is now available!! English 10 Dec 2021
dusty.schafer dusty.…
What is a Subnet Mask? English 10 Nov 2021
jcoleman02 jcoleman02
Resolving Servo Feedback Choices English 04 Nov 2021
kenny.…
Compartilhamento do Barramento DC entre Drives AKD e AKD-C Portuguese, Brazil 03 Aug 2020
Leonardo Souza Leonardo…
AKD and EtherCAT CSV Mode English 02 Apr 2018
Dan.Wolke@Kollmorgen.com Dan.Wolke…
FAQ Seiten German 24 Jan 2018
Will Gaffga Will…
Clearing an AKD-C Power Supply Fault from a PxMM Application Program English 13 Dec 2017
C Wontrop C Wontrop
AKD EtherCAT Max Torque Scaling - Object 6072 German 04 Oct 2017
Matthias.…
Why does the connection on my PC say Limited or no connectivity available and display a warning symbol at the local area connection icon in Windows?

Although Windows displays this message and the limited functionality icon for the drive connection, your PC can communicate fully with the drive. This message and the icon are normal for an AKD to PC connection.

Why does the background color of some of the screens in Workbench appear gray?

This is because you are using the Windows classic theme. To get a white background you must change the theme that Windows is using.

To change the theme go to the Control Panel, select Display, select the Themes tab, and choose a new theme, such as "Windows XP".

Why can't workbench find my drive on the network?

See Device not Shown in the Workbench Help for a detailed discussion of this problem.

Why can't I see my AKD drive when I try to connect in Workbench?

If you are communicating through the Ethernet port at connector X11, you might not see your drive in the connect window for any of the following reasons:

  • Poor cable connection. Make certain you have a good connection between your computer and the drive by checking to see if you see a blinking light next to the connector (at each end).
  • Improper rotary switch setting. Make certain that the S1 and S2 rotary switches on the front of the drive are set to 0 (bottom position), unless you are attempting a point to point connection and your computer is set up to connect in this manner.
  • Conflict with another device that is networked to your computer (including your wireless connection). In some cases, turning off your wireless card will fix this. You can turn your wireless card back on after you establish communication with the AKD).
  • Improper TCP/IP settings. Make certain that the TCP/IP settings in the network port that you are communicating through are working properly.
What if I cannot connect to my drive using WorkBench, but I have been advised to download new firmware to the drive to fix the problem?

In most cases, firmware is downloaded using WorkBench without setting the hardware into a specific “download” state. If you need to download firmware, but are unable to connect to WorkBench, use the procedure described in Forcing the drive into firmware download mode in the Workbench help.

The drive is running rough and noisy after autotuning procedure. What can I do?

Autotuning of your application delivered unexpected results while tuning the current feed forward value. Please deactivate "Tune Acceleration FF" in the Workbench Performance Servo Tuner screen and restart the tuning.

How long does it take until foldback is totally recovered?

Up to 500 s depending on the active current. See page Foldback Times.

How long can the drive sustain a constant current above Icont before faulting?

5 seconds with Ipeak. Smaller currents can be sustained for longer periods. See Foldback Times.

How do I view parameter information from Workbench screens?

There are two ways to find out about what parameter is behind a text box in Workbench.

  1. Right click on the text box and select Parameter Info from the menu. A popup appears next to the window selected. Note if you clicked the Help, you get taken to the page in the help system. Pressing F1 also does the same.
  2. Click the “Tell me more about this topic” link at the top of each page.
How to Change IP Address in AKD-C and AKD-N
kenny.…
March 11, 2022
Does AKD support 400Hz AC Power Supply?
Xinbo.…
February 23, 2022
About Leakage Current of AKD Drive
Ryu
August 17, 2017
Anticollision Arm
Dome
March 18, 2017
Kollmorgen SILVERLINE SERVO MOTOR
Ryu
August 3, 2016
Encoder Connector P/N
Scott…
April 6, 2015