AKD-C/N
The AKD-C Power Supply and AKD-N drives lie at the core of a decentralized drive system. Up to 16 AKD-N drives can be connected to one AKD-C central power supply. Hybrid cables are used to connect the AKD-C to the drives and to daisy-chain the drives. For more specific information about the individual components, see the AKD-C and AKD-N topics.
| Current Firmware Version | 1.20.00.001 |
| Firmware Release Date | December 2020 |
| Current Hardware Revision (AKD-N) | B |
| Current Hardware Revision (AKD-C) | A |
| Hardware Release Date | 01/01/2014 |
| Part Number Scheme | AKD-N (PDF) AKD-C (PDF) |
| See the WorkBench article for details about the software used to configure and manage the drives. | |
| Components | |
|---|---|
| AKD-C | Central Power Supply |
| AKD-N | Decentralized Servo Drive |
Blue Boxes: All components in the blue box are products delivered by Kollmorgen. For detailed information click to the product or use the table below for navigation.
Gray Boxes: Elements in the gray area are components which have to be added by the machine builder.

| AKD-C | AKD-C Power Supply |
|---|---|
| AKD-N | AKD-N Drive |
| AKD-CN-Coupling | Connector interface for cabinet wall (in process) |
| AKD-M | AKD PDMM Drive |
| AKM | AKM Motor |
| AKMH | AKMH Motor |
| AKI | Operating Console |
| AKT | KAS Input and Output Terminals |
| BAR/BAS/BAFP | Brake Resistor |
| Cx Cables | Configured CC/CM/CF cables for connection of the components, refer to the cable part number scheme |
| DDL | Linear motors (on request) |
| ENCP | Ethernet cables |
| Gearhead | Micron Gearheads |
| Heatsink Kit | optional accessory for AKD-N |
| KAS-IDE | KAS System Setup Tool |
| KBM | KBM Motor |
| KCM | KCM Capacitor Module |
| Redi Mount | Adapters to mount Micron Gearheads to AKM motors |
| Workbench | AKD Setup Tool |
| Filter General | English | ||
| Foldback Times | English | ||
| Forming | English | ||
| Transport and Storage | English | ||
| Sine Encoder | English | ||
| Incremental Encoder | English | ||
| EnDat | English | ||
| BiSS | English | ||
| Fuses | English |
Home >
Knowledge Base >
FAQs >
Downloads >