Skip to main content

Kollmorgen Support Network

AKD-C/N

The AKD-C Power Supply and AKD-N drives lie at the core of a decentralized drive system. Up to 16 AKD-N drives can be connected to one AKD-C central power supply. Hybrid cables are used to connect the AKD-C to the drives and to daisy-chain the drives. For more specific information about the individual components, see the AKD-C and AKD-N topics.

Current Firmware Version1.20.00.001
Firmware Release DateDecember 2020
Current Hardware Revision (AKD-N)B
Current Hardware Revision (AKD-C)A
Hardware Release Date01/01/2014
Part Number SchemeAKD-N (PDF)
AKD-C (PDF)
See the WorkBench article for details about the software used to configure and manage the drives.
Components
AKD-CCentral Power Supply
AKD-NDecentralized Servo Drive

Blue Boxes: All components in the blue box are products delivered by Kollmorgen. For detailed information click to the product or use the table below for navigation.
Gray Boxes: Elements in the gray area are components which have to be added by the machine builder.

image

AKD-CAKD-C Power Supply
AKD-NAKD-N Drive
AKD-CN-CouplingConnector interface for cabinet wall (in process)
AKD-MAKD PDMM Drive
AKMAKM Motor
AKMHAKMH Motor
AKIOperating Console
AKTKAS Input and Output Terminals
BAR/BAS/BAFPBrake Resistor
Cx CablesConfigured CC/CM/CF cables for connection of the components, refer to the cable part number scheme
DDLLinear motors (on request)
ENCPEthernet cables
GearheadMicron Gearheads
Heatsink Kitoptional accessory for AKD-N
KAS-IDEKAS System Setup Tool
KBMKBM Motor
KCMKCM Capacitor Module
Redi MountAdapters to mount Micron Gearheads to AKM motors
WorkbenchAKD Setup Tool
Trade Compliance English
Bethany…
KAS v3.07 is now available!! English
dusty.…
What is a Subnet Mask? English
jcoleman02 jcoleman02
Resolving Servo Feedback Choices English
kenny.…
Compartilhamento do Barramento DC entre Drives AKD e AKD-C Portuguese, Brazil
Leonardo…
AKD and EtherCAT CSV Mode English
…
FAQ Seiten German
Will…
Clearing an AKD-C Power Supply Fault from a PxMM Application Program English
C Wontrop
AKD EtherCAT Max Torque Scaling - Object 6072 German
Matthias.…
Why does the connection on my PC say Limited or no connectivity available and display a warning symbol at the local area connection icon in Windows?

Although Windows displays this message and the limited functionality icon for the drive connection, your PC can communicate fully with the drive. This message and the icon are normal for an AKD to PC connection.

Why does the background color of some of the screens in Workbench appear gray?

This is because you are using the Windows classic theme. To get a white background you must change the theme that Windows is using.

To change the theme go to the Control Panel, select Display, select the Themes tab, and choose a new theme, such as "Windows XP".

Why can't workbench find my drive on the network?

See Device not Shown in the Workbench Help for a detailed discussion of this problem.

Why can't I see my AKD drive when I try to connect in Workbench?

If you are communicating through the Ethernet port at connector X11, you might not see your drive in the connect window for any of the following reasons:

  • Poor cable connection. Make certain you have a good connection between your computer and the drive by checking to see if you see a blinking light next to the connector (at each end).
  • Improper rotary switch setting. Make certain that the S1 and S2 rotary switches on the front of the drive are set to 0 (bottom position), unless you are attempting a point to point connection and your computer is set up to connect in this manner.
  • Conflict with another device that is networked to your computer (including your wireless connection). In some cases, turning off your wireless card will fix this. You can turn your wireless card back on after you establish communication with the AKD).
  • Improper TCP/IP settings. Make certain that the TCP/IP settings in the network port that you are communicating through are working properly.
What if I cannot connect to my drive using WorkBench, but I have been advised to download new firmware to the drive to fix the problem?

In most cases, firmware is downloaded using WorkBench without setting the hardware into a specific “download” state. If you need to download firmware, but are unable to connect to WorkBench, use the procedure described in Forcing the drive into firmware download mode in the Workbench help.

The drive is running rough and noisy after autotuning procedure. What can I do?

Autotuning of your application delivered unexpected results while tuning the current feed forward value. Please deactivate "Tune Acceleration FF" in the Workbench Performance Servo Tuner screen and restart the tuning.

How long does it take until foldback is totally recovered?

Up to 500 s depending on the active current. See page Foldback Times.

How long can the drive sustain a constant current above Icont before faulting?

5 seconds with Ipeak. Smaller currents can be sustained for longer periods. See Foldback Times.

How do I view parameter information from Workbench screens?

There are two ways to find out about what parameter is behind a text box in Workbench.

  1. Right click on the text box and select Parameter Info from the menu. A popup appears next to the window selected. Note if you clicked the Help, you get taken to the page in the help system. Pressing F1 also does the same.
  2. Click the “Tell me more about this topic” link at the top of each page.