Skip to main content

Kollmorgen Support Network

AKD-C/N

The AKD-C Power Supply and AKD-N drives lie at the core of a decentralized drive system. Up to 16 AKD-N drives can be connected to one AKD-C central power supply. Hybrid cables are used to connect the AKD-C to the drives and to daisy-chain the drives. For more specific information about the individual components, see the AKD-C and AKD-N topics.

Current Firmware Version1.20.00.001
Firmware Release DateDecember 2020
Current Hardware Revision (AKD-N)B
Current Hardware Revision (AKD-C)A
Hardware Release Date01/01/2014
Part Number SchemeAKD-N (PDF)
AKD-C (PDF)
See the WorkBench article for details about the software used to configure and manage the drives.
Components
AKD-CCentral Power Supply
AKD-NDecentralized Servo Drive

Blue Boxes: All components in the blue box are products delivered by Kollmorgen. For detailed information click to the product or use the table below for navigation.
Gray Boxes: Elements in the gray area are components which have to be added by the machine builder.

image

AKD-CAKD-C Power Supply
AKD-NAKD-N Drive
AKD-CN-CouplingConnector interface for cabinet wall (in process)
AKD-MAKD PDMM Drive
AKMAKM Motor
AKMHAKMH Motor
AKIOperating Console
AKTKAS Input and Output Terminals
BAR/BAS/BAFPBrake Resistor
Cx CablesConfigured CC/CM/CF cables for connection of the components, refer to the cable part number scheme
DDLLinear motors (on request)
ENCPEthernet cables
GearheadMicron Gearheads
Heatsink Kitoptional accessory for AKD-N
KAS-IDEKAS System Setup Tool
KBMKBM Motor
KCMKCM Capacitor Module
Redi MountAdapters to mount Micron Gearheads to AKM motors
WorkbenchAKD Setup Tool
Splitter-Adapter German
…
Gegenstecker German
…
Netzfilter German
…
KCM Kondensatormodul German
…
Inkrementalgeber mit Hall German
…
Normen und Richtlinien German
…
Stopp und Not Halt Funktion German
…
Inkrementalgeber German
…
Gleichlauf German
…