When it comes to exoskeletons, motion design and motor selection are make-or-break steps in the engineering process. Here we explore key considerations and insights for success.
Humanoid robots are projected to become a $6+ billion opportunity within the next 10 to 15 years.1 Many labs, research entities and startup companies have taken notice, and are rushing to develop concepts and prototypes ahead of the competition. But…
In a short time, humanoid robots have progressed from science fiction to a $6+ billion opportunity. Learn how to succeed in this exponentially growing market by solving motion challenges far beyond the requirements of conventional industrial robots.
From maintenance and repair of deep-sea infrastructure to inspection of wastewater basins. From hazardous oil and gas locations to dirty and dangerous construction sites. From research sample collection to search and rescue in disaster areas. In…
Learn how robot-ready frameless motors from Kollmorgen enable faster, more dynamic agricultural robots that increase farm productivity and profitability.
As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.
What if you could design and build a surgical robot that help doctors perform less invasive, more precise operations and achieve better patient outcomes? While the results of any surgery depend on the challenges of the specific case and the skill of…
An alternative to customizing a servo motor is utilizing a frameless motor and integrating directly into the machine itself. Learn more in our new blog post!
In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…
The new AKME Series for hazardous locations brings ATEX and IECEx certifications, unprecedented compactness and versatility. Compare AKME against Goldline EB.
Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…
As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.
Servo motors are used in numerous markets to power machines, instruments, robots, and other factory automation applications. This blog addresses five major elements of a conventional brushless DC servo motor: the rotor, stator, bearings, feedback and…
When designing motion for applications such as vertical gantries and hoists, you need to take special care to ensure operator safety and operational efficiency. Let’s discuss best practices for meeting the particular challenges involved.
Advances in processor technology for servo drives continue to expand the features and capabilities they offer. Choosing a new drive or control system over an existing system ultimately depends on the application requirements. The AKD2G servo drive…
Every machine designer wants to deliver the best possible performance. Especially in today’s food and beverage industry, the pressure for optimum throughput and quality means that every OEM is striving to engineer new systems that are the best of the…
When learning about servo motors and servo systems, you’re likely to encounter the phrase “closed-loop system.” If you’ve ever wondered what that means and how it works, you’ve come to the right place. Let’s step through some of the most common…
The Low Voltage Directive defines low voltage from 50 – 1000 Vac, or 120 – 1500 Vdc, which is based on the mains voltage used to power the electrical system and ties in with specific IEC regulations on safety and risk of shock and arcing. When low…
When and how to customize a standard servo motor depends on the predicted benefits derived from the customization that should include a solution tied to form, fit, and function. Learn more.
Electro-Optical/Infrared (EO/IR) Systems are used to provide long distance visual and thermal imaging for a variety of applications. Often used in satellites, planes, and military applications, there are two main components found in EO/IR systems:…
When most engineers think of a brushless DC servo motor, they’re likely to visualize a housing with a flange to accept mounting bolts, connectors to accept power and data cables, and a rotor shaft that couples to the load. That’s the most common…
When it comes to exoskeletons, motion design and motor selection are make-or-break steps in the engineering process. Here we explore key considerations and insights for success.
Humanoid robots are projected to become a $6+ billion opportunity within the next 10 to 15 years.1 Many labs, research entities and startup companies have taken notice, and are rushing to develop concepts and prototypes ahead of the competition. But…
In a short time, humanoid robots have progressed from science fiction to a $6+ billion opportunity. Learn how to succeed in this exponentially growing market by solving motion challenges far beyond the requirements of conventional industrial robots.
From maintenance and repair of deep-sea infrastructure to inspection of wastewater basins. From hazardous oil and gas locations to dirty and dangerous construction sites. From research sample collection to search and rescue in disaster areas. In…
Learn how robot-ready frameless motors from Kollmorgen enable faster, more dynamic agricultural robots that increase farm productivity and profitability.
Low Earth orbit (LEO) is a quickly growing commercial economy, and Kollmorgen has the expertise and space-worthy motors to support this new race to space.
What if you could design and build a surgical robot that help doctors perform less invasive, more precise operations and achieve better patient outcomes? While the results of any surgery depend on the challenges of the specific case and the skill of…
Engineers often face challenges when incorporating servo motors into a new machine design. Choosing between a housed motor or a frameless torque motor shouldn’t be one of them. This blog reveals three design considerations that indicate why a…
No two projects are the same, and it’s important to be able to provide a modular solution that can be adapted to suit the customers’ requirements. Learn how Heli created specialized high-reach AGVs equipped with Kollmorgen technology to meet their…
In factories and warehouses, we have these clever machines known as Automated Guided Vehicles (AGVs) and Autonomous Mobile Robots (AMRs). They're changing the way we manage materials by doing tasks on their own, making manufacturing and warehousing…
In the ever-evolving landscape of manufacturing, innovation stands as the cornerstone of progress. New Pearl Group, a pioneering force in the ceramics industry, has taken a significant leap forward by embracing intelligent production techniques.…
In today's rapidly evolving world of automated guided vehicle (AGV) systems, staying ahead of the competition requires continuous learning and skill development.
Could prompt AI such as ChatGPT, Google Bard or Microsoft CoPilot revolutionize the AGV arena? Sebastian Witkarsson, Information Security Officer at Kollmorgen, examines the possibilities – and sounds a note of caution.
Kollmorgen is all about innovation, constantly investing in collaborations and research projects to exchange knowledge and expertise with partners and universities across the world. Learn more about how Kollmorgen works to enable innovative thinking…
At Kollmorgen, there are more and more female employees every year, which really helps to broaden overall perspectives. Everyone agrees that diversity drives innovation and these values apply to the group at every level.
We are now living in a digital world. E-commerce consumers expect goods to be delivered faster and more flexibly than was the case just a couple of years ago. Organizations, retailers, and their warehouse service providers therefore need to find new…
Accessible and affordable automation for all has made a giant leap forward with the release of an AMR platform that enables users to install out-of-the box automation technology in less than a day.
We are no longer settling for unsustainable. More than ever before, we are painfully aware that our ability – or inability - to act over the next few years will directly shape the lives of all future generations. And our best bet to step up to the…
Machine Learning, Neural Networks – big terms in modern logistics, but what do they actually mean? What we need is an expert to tell us. Paul Hamblin, editor of Logistics Business magazine, meets one.
The purpose of an AGV system is efficient transportation of goods in a specified environment. The AGV system is a big investment, so it is desirable to have a high degree of utilization as well as a high ratio of deliveries per hour to get a good…