Skip to main content
blog | Greater Comfort & Safe Mobility in Exoskeleton Design |
|
2 minute read

The exoskeleton market is at a tipping point. With an aging population, increases in chronic disease and no end in sight for serious labor shortages, exoskeletons offer tremendous potential. In fact, market reports estimate that the exoskeleton market will grow at a compound annual growth rate of nearly 40% between now and 2028 — when it will reach $3.7 billion.

Engineers are currently hard at work to develop exoskeletons that help restore movement for those with motor impairments and even augment natural human performance. But the segment isn’t without its challenges. As wearable devices, exoskeletons must be comfortable, reliable and safe — a tall order given their extremely complex mechanics.

Engineers must consider three main criteria when designing exoskeletons for commercial viability: temperature, safety and mobility.

Keeping Operating Temperatures Low

Engineers know all too well that heat generated from motors can become a major issue in temperature-sensitive applications. In **exoskeleton design**, however, engineers don’t have many traditional motor-cooling options because of strict size and weight limits, including:

- Fans  
- Water cooling  
- Insulation  

Typical motors can operate at a maximum winding temperature of 155°C (over 300°F), but motors used in exoskeletons must perform reliably at much lower temperatures—without the cooling methods listed above. The challenge is that engineers are often offered frameless motor designs made for industrial robotics applications, and these can run at temperatures that exceed what’s practical for exoskeleton equipment, especially since the device sits close to the user’s body.

Instead, engineers need thermally efficient motors that can operate at roughly 50–60°C to reduce the impact of close-to-body contact. The tradeoff is that these lower winding temperatures can significantly reduce the performance of typical frameless motors. To plan effectively, engineers should work with a partner that provides both thermally efficient motors and motion design tools that can simulate motor performance at specific:

- Torque requirements  
- Speed ranges  
- Temperature limits  

This makes it easier to plan for different application needs and determine the right motor sizing requirements.

Sizing for Safety & Mobility

One of the biggest hurdles to viable exoskeleton design is sizing. Not only must engineers account for the sizing differences inherent in the human population, but they must also keep their designs as slim, streamlined and lightweight as possible to allow for maximum comfort, safety and mobility.

Particularly in medical rehabilitation applications, engineers must account for the fact that a user may have little to no function in certain limbs. Here, lighter-weight designs are crucial to ensure safety in the case of falls or accidents.

Lighter-weight designs are also important for comfort, especially if OEMs hope to widen exoskeleton adoption, and for applications that require more sustained or regular use of the exoskeleton. For example, workers and patients using exoskeletons for rehabilitation or mobility will not be willing to endure excessive weight or uncomfortable pressure on the body. In addition to discomfort, designers must account for and reduce common risks to the wearer, including:

  • Injury or discomfort caused from friction/direct contact between the exoskeleton and the user
  • Joint hyperextension and overexertion
  • Unintended contact, collision, and vibration exposure

Finally, streamlined, sleek designs are a must to allow the user to navigate tighter spaces and to reduce the risk of the exoskeleton snagging on nearby objects.

These strict size and weight considerations require frameless motors that are compact yet powerful enough to meet the needs of the given exoskeleton application.

Motors Designed for Exoskeletons

The majority of high-performance, frameless motors are designed for general automation or, at best, robotic joint applications — and therefore may not meet the more intensive demands of exoskeleton designers. Kollmorgen’s TBM2G motors, however, were made for the task.

They deliver consistent torque across the full range of speed — all in a more compact package. Engineers will enjoy high performance within the required temperature range, without having to oversize the motor. TBM2G motors were made to integrate easily with harmonic-drive-type mechanisms most commonly used in exoskeleton joints, with optional integrated Hall sensors that don’t increase motor length.

Finally, TBM2G motors come in seven diameters ranging from 50 mm to 115 mm and three stack lengths ranging from 8 mm to 26 mm — so exoskeleton OEMs can more easily scale to meet varying human sizes and application requirements.

Choosing the Right Partner

When it comes to exoskeleton engineering, selecting the right partner is as important as the design components themselves. As the exoskeleton market quickly develops, Kollmorgen can help engineers stay ahead of the curve.

Kollmorgen is the global leader in frameless, brushless motor design and manufacturing — with the motor selection, engineering guidance and service to support any exoskeleton application.

Contact us to discuss your needs and goals with a Kollmorgen exoskeleton expert.

Consult an Expert

Frameless Motors

Discover Kollmorgen's frameless motor range, designed for easy integration into your application, enhancing performance, efficiency and reliable motion solutions.
Learn More

TBM2G Series Frameless

These next-generation frameless motors deliver high torque density for your most compact, lightest electromagnetic package, standard sizing for harmonic gearing, and scalable design to keep you on top of your global production needs.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
Designing Field Robots for Harsh and Unpredictable Environments

Designing Field Robots for Harsh and Unpredictable Environments >

This session explores how innovative technologies from Kollmorgen and Regal Rexnord’s broad portfolio of motion control technologies can help engineers meet the rigorous demands of field robotics.
Motion Control Principles for Scalable Humanoid Robotics

Motion Control Principles for Scalable Humanoid Robotics >

As humanoid robotics gain momentum across industries—from logistics and manufacturing to healthcare and public safety—the demand for precise, efficient, and scalable motion control solutions is accelerating. Engineers face complex challenges in…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.