Skip to main content
blog | How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? |
|
2 minute read

Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

Servo systems depend on closed-loop feedback motor control to determine the rotor’s position at any given moment. The drive uses this motor feedback loop to properly commutate the motor phases, precisely controlling its torque, position and speed according to the application requirements.

Why encoder failures can cause unsafe, unpredictable servo motion

Although encoders are generally highly accurate and reliable, there are several conditions that can potentially cause errors in rotor position or even the direction of rotation. These errors can be large and catastrophic or small and cumulative. For example, an encoder can break outright or gradually fail over time, sending increasingly erroneous signals.

In a manufacturing environment, the consequences of a failed feedback device may be limited to unplanned downtime and wasteful scrap — undesirable outcomes, but not necessarily dangerous. However, there are many applications where failure of the motor feedback loop is simply not an option.

For example, in a medical environment, a failed encoder could endanger patients and staff by causing unpredictable motion of equipment such as a patient table or radiotherapy gantry, or by causing a pump to deliver improper flow of a fluid. And there are many other industries and applications that depend on fail-safe servo motion.

The U.S. Food and Drug Administration regulates medical devices to ensure their safety and effectiveness, including recommending redundant measures to ensure correct and accurate operation of critical systems. Even when there’s no clearly defined regulatory framework, redundant feedback is a best practice to ensure absolute reliability of the servo system.

How traditional external redundant feedback works

To achieve redundancy, OEMs often add a secondary feedback device to validate the reliability of the main feedback device. Typically, this is achieved by specifying a servo motor that incorporates an encoder and pairing that with an external feedback device added somewhere along the driven shaft or load.

Both devices are wired to the servo drive, and the added device serves the purpose of verifying the direction of rotation and the approximate position being reported by the main device. If one feedback device indicates clockwise rotation while the other indicates counterclockwise, or if they differ significantly in speed or position, the drive knows a failure has occurred and can take appropriate action.

This dual-loop feedback results in extremely reliable motion — but at the expense of significantly greater complexity and cost. The design footprint must be enlarged to accommodate the redundant feedback device. Routing an additional set of feedback cables from a separate location can be challenging. And assembly of a more complex motion system can be difficult and time-consuming.

How integrated redundant feedback simplifies design and boosts safety

Kollmorgen offers an extensive range of standard product modifications that deliver highly specialized capabilities in products that can be rapidly prototyped, are highly manufacturable, and don’t require customers to assume the risks or cost of a custom product.

One of these standard modifications is the ability to build both an absolute encoder and a Hall effect sensor into the same motor without significantly altering the overall motor dimensions. With dual motor feedback loops integrated into the motor, you don’t have to find a place on the motor shaft or external load to add a second feedback device, and you can keep the dimensions of your application as compact as possible.

With redundant feedback devices integrated into the motor, Kollmorgen also offers a single cable that carries both the encoder and Hall effect sensor feedback signals to the drive. This saves the material and labor costs that would otherwise be required for routing two separate cables and allows you to further minimize the footprint of your machine design.

Plus, with a fully integrated solution, you gain confidence that the entire motion system benefits from the power, precision and reliability that only Kollmorgen can offer.

Our customers have already used this solution in modified AKM motors that drive critical systems in surgical robots, patient tables, medical pumps and more. What’s your application, and how critical is it to ensure fail-safe feedback for can’t-fail motion?

Contact us today, and let’s solve your specialized application requirements, engineer to engineer.

Consult an Expert

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

AKM™ Series Servo Motor

Our best-in-class, high-performance servomotors offer a wide range of mounting, connectivity, feedback and other options. More than 500,000 standard models are available along with co-engineered modifications to suit almost any application requirement.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Driving Aerospace & Defense Innovation with Motion Technology >

Motion technology is the execution layer that turns AI and software into physical mission readiness. Explore how it drives aerospace and defense innovation at scale.
Space satellite

Engineering Motion Systems for Space: A Guide to Reliability, Scalability and Mission Success >

Move from terrestrial prototypes to mission success with a practical guide on evaluating space-ready motors and engineering spacecraft motion control.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
Designing Motion Control for Turrets and Large Azimuth Drive Systems in Military Ground Vehicles

Designing Motion Control for Turrets and Large Azimuth Drive Systems in Military Ground Vehicles >

It’s important to distinguish between technology and topology when designing motion systems for large military ground vehicles. Topology is the high-level architecture of how those components are arranged and interact within your system.
Motion Design for Next-Generation Armored Fighting Vehicles

Motion Design for Next-Generation Armored Fighting Vehicles >

Learn what to consider when designing for next-gen armored fighting vehicles, from electromechanical motion architectures to mission-critical performance.
Technology vs. Topology: Designing Motion for Turrets and Large Azimuth Drive Systems

Technology vs. Topology: Designing Motion for Turrets and Large Azimuth Drive Systems >

Learn how to select the right motion system topology for your ground vehicle platform and go from concept to combat success with Kollmorgen.
Enhance Defense System Development with Advanced Motion Design

Enhance Defense System Development with Advanced Motion Design (Turkey) >

Optimizing the form factor and ensuring the reliable function of your defense system design is crucial. As you think about your design, Kollmorgen and its partner brands under the Regal Rexnord banner can help you build success by delivering…
Mastering Motion: A Comprehensive Tour of the Modern Surgical Robot Suite

Mastering Motion: A Comprehensive Tour of the Modern Surgical Robot Suite >

Step into the future of surgical robotics and enhance your understanding of what’s possible. This webinar offers a detailed exploration of the cutting-edge components that drive precision and efficiency in today's advanced surgical robots.
Enhance Missile Development with Advanced Motion Design

Enhance Missile Development with Advanced Motion Design >

This webinar will discuss the critical motion control elements needed for effective missile development and how these elements can work effectively together — from motors of all sizes to ball screws, resolvers, brakes, bearings and seals, to…