Skip to main content
blog | Stacking 3-ton pallets of soft bags: No challenge for Kollmorgen-equipped AGVs from Heli |
|
2 minute read

No two projects are the same, and it’s important to be able to provide a modular solution that can be adapted to suit the customers’ requirements. Learn how Heli created specialized high-reach AGVs equipped with Kollmorgen technology to meet their customers’ needs of stacking heavy pallets of soft bags, while improving efficiency and safety.

As part of a smart automated manufacturing initiative, one Chemical Company decided to implement automated guided vehicles (AGVs) in the warehouse at their urea manufacturing plant in Xinxiang, China. The AGV fleet is tasked with moving heavy pallets of soft bags with fertilizers from the packaging facility to the storage area, and subsequently to the outbound goods area. This enabled them to increase efficiency and safety, while achieving 24-hour operation with a constant and more predictable throughput.

Spearheading this initiative, Heli implemented specialized high-reach AGVs in the warehouse, harnessing the power of Kollmorgen NDC Solutions for order routing, traffic management, vehicle navigation, and control. Utilizing laser navigation technology with reflectors over a robust 5G network, the AGVs efficiently process orders received from the Warehouse Management System (WMS), ensuring streamlined operations.

One of the requirements in this project involved the need for AGVs to stack two tiers of pallets with soft bags. With individual pallets weighing up to 3 tons, the varied compression of bag contents on each lower pallet could pose a challenge. To manage this, the AGVs were equipped with high-precision fork sensors, enabling them to execute loading and unloading tasks with a flexible position tolerance.

The Chemical Company has declared that the automation initiative is a great success. The implementation took less than 6 months from project start to an operational site, with the final AGV commissioning being completed in 45 days. Heli’s AGVs with Kollmorgen technology enables safer operation with reduced damage to goods and equipment, and higher precision and efficiency—resulting in 60% cost savings.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…