Skip to main content
blog | Why Consider Frameless Motors for Customized Solutions |
|
2 minute read

Conventional machine designers typically focus on selecting an off-the-shelf, housed motor to establish the motion axes. Occasionally, a designer will modify a standard motor’s physical dimension, windings, or combinations of both, to customize to an application. An alternative to customizing a servo motor is utilizing a frameless motor and integrating directly into the machine itself.

KBM Motors Group

Frameless motors consist of a rotor and stator set that, when combined with a feedback element, offer significant advantages when integrated directly into the machine actuators. While assembling a frameless motor may seem difficult, the process is actually similar to the other assembly requirements of machine construction.

Why would a machine designer use a frameless motor solution over a conventional housed design? A frameless motor design makes sense when considering:

  • Performance Optimization
  • Environmental Factors
  • Aftermarket Revenue
  • Intellectual Property Protection
  • System Cost Reduction

Performance: Integration of a frameless motor into a machine provides several performance advantages. Integrating the motor directly to a rotating shaft element can reduce overall system inertia. Reduced inertia also reduces the torque required to accelerate and decelerate the motor which, in turn, improves move and settling times to increase system bandwidth. Frameless motors have similar winding options as standard motors and can also be customized to optimize performance. Machine performance optimization provides the machine builder with advantages to potentially differentiate their machine from the competition.

Environment: Motion actuation design may require a machine designer to manage specific environmental factors. For example, the incorporation of a frameless motor into a sealed housing that is required for other mechanical and environmental elements can lead to the simplification of the overall machine design. Standard housed motor designs are typically rated for an industrial environment and can handle typical factory dust and heat. When special environments are encountered, however, such as extreme heat or cold, vacuum, radiation, or caustic washdowns, it is then necessary to customize the motor to meet the specific environmental challenges. Frameless motors offer a large variety of options to integrate the motor to both the machine and the required environmental conditions.

Kollmorgen Engineers Collaborating

Aftermarket Revenue: The integration of a frameless servo motor into a machine design results in a proprietary incorporation of the motion elements into the machine builder’s overall design. The new configuration of the motor elements is now “owned” by the machine builder and requires the end user to purchase spares directly from the builder, which protects aftermarket sales. This frequently overlooked benefit provides an increased revenue stream over the life of the machine design.

Intellectual Property Protection: A compelling reason to consider frameless designs is that a customized frameless servo motor design provides unique functional capabilities that may be patentable (or are easily protected).

Cost Reduction: The elimination of the standard housed motor design elements that are not required for the specific application can help reduce the unit cost of the motor, even when upfront costs are considered. Certain standard features, such as sealing, connectorization, or feedback elements, can be integrated into the machine assembly to eliminate extra housings, bearings, couplings, and other elements that are required when using a housed motor.

Conclusion

When deciding to use a frameless motor to customize machine motion elements, the designer needs to consider the overall machine performance, ease of assembly, and feature requirements. A frameless motor integrated into a machine design can add a competitive advantage over a standard housed motor solution to increase sales. When considering the integration of a frameless servo motor into a machine design, looking at vendors that excel in motor development and design capabilities is paramount. An experienced vendor, such as Kollmorgen, acts as an extension of the customer’s engineering team to help obtain the best solution for the machine builder’s needs.

Consult an Expert

Frameless Motors

Discover Kollmorgen's frameless motor range, designed for easy integration into your application, enhancing performance, efficiency and reliable motion solutions.
Learn More

TBM2G Series Frameless

These next-generation frameless motors deliver high torque density for your most compact, lightest electromagnetic package, standard sizing for harmonic gearing, and scalable design to keep you on top of your global production needs.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scalable Humanoid

The Scalable Humanoid Robot >

A successful prototype may prove a concept, but the actuator architecture determines if it can scale. This gap is why many humanoid programs stall when transitioning from working prototype to manufacturable product.

Driving Aerospace & Defense Innovation with Motion Technology >

Motion technology is the execution layer that turns AI and software into physical mission readiness. Explore how it drives aerospace and defense innovation at scale.
Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Space satellite

Engineering Motion Systems for Space: A Guide to Reliability, Scalability and Mission Success >

Move from terrestrial prototypes to mission success with a practical guide on evaluating space-ready motors and engineering spacecraft motion control.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.