Skip to main content
blog | How to design EO/IR motion control that survives harsh environments: 5 conditions to plan for |
|
2 minute read

Electro-Optical/Infrared (EO/IR) Systems are used to provide long distance visual and thermal imaging for a variety of applications. Often used in satellites, planes, and military applications, there are two main components found in EO/IR systems: sensors and the motion system. The sensors, cameras, etc. need to operate during the day and night in many environmental conditions to present a clear image. The motion control (motors) of an EO/IR system must provide smooth, error free movement in the azimuth and elevation axes. While both the sensors and motion systems need to be reliable in many environmental conditions, let’s take a look at the 5 Harshest Environments for EO/IR Motion Control Systems.

1) How do fog and rapid altitude/pressure changes affect EO/IR motion control?:

For EO/IR systems the concerns for clouds and fog are not only around the ability for the system to see. The EO/IR sensors are usually mounted on a platform that moves and when entering clouds and fog, these movable objects are then susceptible to the moisture in the air as well as any air pressure changes (especially for high altitude uses). To ensure that the movements of these platforms will continue to operate after the introduction of wet conditions, special attention is paid to the motion system. It will need to resist rust and work with air pressure changes. Motion suppliers need to pass military standard 810 G testing for humidity and altitude. (MIL-STD 810 G 506.5)

2) When does humidity become a thermal problem for EO/IR targeting accuracy?

Like fog, humidity introduces liquid to the motion control of the EO/IR system. Humidity also makes heat dissipation more difficult as the motion control system works to handle the changes in the torque needed for accurate targeting. The further away from the desired target, the more precise the angular degree of rotation will need to be in order keep the object visible. Motion systems need to continue working in the moist environments and torque feedback will need compensate for additional heat. (MIL-STD 810 G 507.5)

3) How does vibration interfere with motion accuracy and system reliability?

Vibration is a condition of the environment, both in transportation of the EO/IR components as well as when the system is connected to an operating platform. Vibration is motion. It’s never a friend to motion control systems. This extra motion can cause loose connections within a system, airgap differences between rotor and stator, and feedback issues during motion correction. In short, using a rugged motion control system is necessary to mitigate the effects of vibration. Vibration is usually a part of an EO/IR system on a moving platform whether aerial, naval, celestial, or terrestrial. (MIL-STD 810 G 514.6)

In addition, using the motion control system to mitigate vibration in the system (also known as motion/image stabilization) allows for clear target identification. Image stabilization works by counter-acting the vibration using the motion control system to move in equal but opposite directions thus providing a neutral motion environment. (No MIL-STD, but awesome none-the-less)

4) How does sand ingress threaten EO/IR motion control components?

It gets everywhere. It’s also relentless. We’re essentially trying to keep small particles out of the EO/IR motion system. Generally, the design of the EO/IR system would prevent sand and particles from ever reaching the motion system, but even the motors will need to pass MIL-STD 820 G 510.5.

5) Why is salt exposure uniquely risky for EO/IR motion systems and electronics?

Like sand, it gets everywhere. It’s also very corrosive. Motion systems susceptible to salt and corrosion will require prevention and, at the motor level, may include special coatings. In addition, salt is an electrolyte, which can affect the electronics within a motion system. Understanding the ramifications of salts and other corrosives to the motion system and how to prevent corrosion and unwanted electrical activity is a key discussion to have with a motion system supplier. (MIL-STD 820 g 509.5)

Do you agree with Top 5 Harshest Environments list or would you change any of these top 5?

 

Consult an Expert

Frameless Motors

Discover Kollmorgen's frameless motor range, designed for easy integration into your application, enhancing performance, efficiency and reliable motion solutions.
Learn More

TBM Series Frameless

Our TBM series provides direct drive frameless motors designed to be directly embedded in the mechanical structure of your systems, minimizing weight, size and inertia without sacrificing performance.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Driving Aerospace & Defense Innovation with Motion Technology >

Motion technology is the execution layer that turns AI and software into physical mission readiness. Explore how it drives aerospace and defense innovation at scale.
Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Space satellite

Engineering Motion Systems for Space: A Guide to Reliability, Scalability and Mission Success >

Move from terrestrial prototypes to mission success with a practical guide on evaluating space-ready motors and engineering spacecraft motion control.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
RBE Series Motors Selection Guide

RBE Series Motors Catalog >

The RBE series brushless motors provide a wide range of flexible motor solutions for frameless DDR (Direct Drive Rotary) motor applications. These motors come in either housed (RBEH) or frameless (RBE) mechanical configurations.
Designing Motion Control for Turrets and Large Azimuth Drive Systems in Military Ground Vehicles

Designing Motion Control for Turrets and Large Azimuth Drive Systems in Military Ground Vehicles >

It’s important to distinguish between technology and topology when designing motion systems for large military ground vehicles. Topology is the high-level architecture of how those components are arranged and interact within your system.