Skip to main content
blog | What is Considered a Low Voltage Motor? |
|
2 minute read

Blog - What is considered a low voltage motor?

This is a tricky one to answer – the Low Voltage Directive defines low voltage from 50 – 1000 Vac, or 120 – 1500 Vdc, which is based on the mains voltage used to power the electrical system and ties in with specific IEC regulations on safety and risk of shock and arcing. When low voltage motors are discussed in the context of servo motors however, low voltage is focused on battery operated applications. While standard industry brushless motors are typically operated at 120 – 480 Vac, low voltage servo motors are optimized at voltages ranging for 24 – 96 Vdc. By definition, voltages in this range are considered by the IEC to be in the Extra Low Voltage (ELV) category.

What makes a motor low voltage? 

A servo motor is powered by a drive that obtains power from either an AC or DC source. Two specific motor parameters determine the motor’s speed/torque characteristics – the back EMF (Kb) measured in Volts/krpm, and torque sensitivity (Kt)measured by Nm/A. The motor speed is directly related to the applied voltage, and the motor torque is directly rated to the applied current. These two characteristics are directly affected by how many turns of wire are used in the motor coils, with the motor winding typically optimized for the voltage intended for the application. A motor can operate at voltages up to its maximum voltage rating, which is based on the insulation system used in the motor construction.

Example: A motor rated at 2000 rpm with a rated torque of 5 Nm will utilize windings with 10 turns per coil having a voltage rating of 170 Vdc and current rating of 10 A. If this motor was powered with 85Vdc and no adjustments were made to the winding, it would only be capable of 1000 rpm at 5 Nm (assuming the same current is available at the lower voltage). To operate at the same power level with a lower voltage, the motor winding would be adjusted by reducing the number of turns (5 turns per coil) to achieve 2000 rpm at 85 Vdc. However, doing this changes the motor torque sensitivity characteristics and, to achieve 5 Nm of torque at 2000 rpm with 85 Vdc, 20 amps will now be required.

AKM2G-32ML Graph

Consider typical battery-operated applications, such as remotely operated vehicles (ROV’s) or Robotics, where voltage from 24 – 96 Vdc are utilized. The servo motor would need to contain windings that were optimized to meet the load point at the specific applied voltage and available current. These applications are ideal for low voltage motor solutions since the application requirements are typically lower speeds and higher torque. However, a low voltage motor may be applicable for operation at higher speeds as well if the motor windings are optimized for efficient operation at the rated speed, torque, available voltage and current.

Consult an Expert

AKME Series Servo Motors

AKME Series is built on the AKM platform and designed for use in Zone 2 and Zone 22 environments with ATEX and IECEx global certification.
Learn More

AKMA Servo Motors

The lightweight AKMA servo motor is designed for harsh environments like food and beverage processing, and delivers performance and reliability.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When should you convert from a stepper motor to a servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
Automatic Pick and Place machine installing components on circuit board

How mechatronics design improves motion system performance >

Discover how mechatronics design boosts motion system performance by integrating servo systems and control for faster commissioning and integrated motion.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple

Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple >

Introducing Kollmorgen’s AKME servo motors—ATEX/IECEx certified and engineered for compact, versatile performance in hazardous environments where choices have been limited—until now.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK
Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español)

Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español) >

Descubre cómo Kollmorgen Essentials ofrece control de movimiento de alta precisión y fiabilidad comprobada, ahora más rápido de configurar, más fácil de integrar y más rentable de escalar.
Español
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.