Skip to main content
blog | What is a Closed-Loop System? |
|
2 minute read

When learning about servo motors and servo systems, you’re likely to encounter the phrase “closed-loop system.” If you’ve ever wondered what that means and how it works, you’ve come to the right place. Let’s step through some of the most common questions.

What is a closed loop? Aren’t loops always closed?

When you visualize some familiar loops we see around us—roller coasters, racetracks, key rings—they all share a basic characteristic: The end meets back up with the beginning. The same concept can apply to servo loops. The control system issues a command to the drive; the drive sends power to the motor; and the motor’s response—speed and position—are communicated back to the control system, closing the loop. The goal is for the feedback to match the command.

But what, technically speaking, closes a servo motor loop? 

The one-word answer engineers often give is “feedback,” but this is only partially true. Closed-loop systems do rely on devices that provide torque, speed and position feedback, but the loop is only closed after the control does something with the feedback data.

For example, the drive control issues a command, or rather a target, telling the drive to move the motor at 1,500 rpm. The drive energizes the motor, and the motor responds. But if the feedback device communicates to the control that the motor is only moving at 500 rpm, the drive control registers an error. Here lies the heart of the servo system. Recognizing that 500 rpm is not correct, the drive control makes a new calculation for what it would take to get the motor to spin 1,500 rpm and adjusts the current accordingly.

So, what’s happening inside the drive to close the feedback control loop?

The loop is closed as feedback data enters a summing junction in the control system that calculates an error—the difference between the target and the actual—and the drive control issues a new command to compensate. All of this can happen very quickly, hundreds of times faster than the blink of an eye, and the process repeats continuously.

But what if I want to regulate something else, like torque or position versus velocity control?

For a servo system there are multiple loops. The primary loop is the current loop. Current translates to torque at the motor. The current loop in the drive receives a command, then sends current to the motor. The sensing device inside the drive measures the current and sends the value back into the summing junction. If an error exists, the drive adjusts to correct the current. But what if the target current is not correct to achieve the target velocity and/or position? This is why there are additional loops.

The second loop is the velocity loop. The feedback for this loop is typically attached to the motor or the object in motion. The feedback is sent back to the drive control. The difference here is that if a velocity error exists, the control issues a new current command into the primary current loop. In other words, the velocity loop feeds its error into the current loop. As the current changes, velocity changes, and both loops review the feedback data for errors.

The third loop is the position loop. As you can imagine, the process is the same. Target position compared to actual position results in a position error that gets sent to the velocity loop as a new command. The velocity loop works as described above to provide a target current. The three loops work simultaneously to achieve the target position. 

Servo Motor Diagram 

To summarize, in order to regulate position, velocity, torque or another system parameter like pressure or tension, there must be associated feedback into one of the control loops so that the loop can be closed.

If we call this a closed-loop system, can there be an open-loop system?

Although it’s common to see the term open-loop, this could be considered a misnomer since it really means “no loop.” The reality is the loop doesn’t exist until we close it with feedback.

In an open-loop system you have an expectation of the outcome, but since you are not measuring it you really don’t know what is happening at the load. You could take an inherently open-loop system, like a stepper system, and add a feedback device for position or velocity. Essentially, you’re recognizing that potential loops exist, and you’re closing them. This does happen, and it’s why you’ll see feedback devices for steppers—usually with the phrase “servo-like” somewhere in the product description.

But then the question becomes, if you’re taking a stepper motor and closing one or more loops:

At what point should you just go with a servo system?

Good question. That’s when you should consider contacting a motion expert to discuss your specific application needs.

Consult an Expert

AKME Series Servo Motors

AKME Series is built on the AKM platform and designed for use in Zone 2 and Zone 22 environments with ATEX and IECEx global certification.
Learn More

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When should you convert from a stepper motor to a servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
Automatic Pick and Place machine installing components on circuit board

How mechatronics design improves motion system performance >

Discover how mechatronics design boosts motion system performance by integrating servo systems and control for faster commissioning and integrated motion.
Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple

Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple >

Introducing Kollmorgen’s AKME servo motors—ATEX/IECEx certified and engineered for compact, versatile performance in hazardous environments where choices have been limited—until now.
Introducing the latest update to SafeMotion monitor firmware - SMM 3

Kollmorgen advances linear motor safety and performance with SafeMotion Monitor firmware upgrade >

The latest SafeMotion Monitor™ firmware (SMM 3.0) expands functional safety for linear motors with EnDat 2.2 safe feedback support and SIL 3 compliance.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK