Skip to main content
blog | How Does Kollmorgen Utilize Data Analytics for AGVs? |
|
2 minute read

How Does Kollmorgen Utilize Data Analytics for AGVs?

The purpose of an AGV system is efficient transportation of goods in a specified environment. The AGV system is a big investment, so it is desirable to have a high degree of utilization as well as a high ratio of deliveries per hour to get a good ROI.

Searching for clues

Kollmorgen measure the performance and behavior of AGV systems, both on a system level and on board individual AGVs. We collect information on motor drives, laser scanners, localization, traffic, and obstacle interference.

By collecting data Kollmorgen finds trends and patterns, which can be used to improve the products and develop the best possible configuration for any given AGV system. Highs and lows in productivity, daily utilization trends etc. is measured, and the data is used to optimize routes, increase throughput and calculate smarter resource utilization. To the end-user, this translates into lower costs and higher revenue.

The collected data can also give important clues to external processes that might disturb AGV performance. For example, pedestrians getting in the way of the AGVs, or manual forklifts driving in areas originally planned primarily for the AGVs.

Leveraging data and creating benefits

Analysis of the collected data helps reveal inefficiencies of in the AGV route network of a particular site. By aggregating data from multiple sites, Kollmorgen system users can identify deviating individuals, models or components in their AGV fleet. The collected data is stored in a SQL database, accessible in NDC8, offering a dashboard with visualizations of system level KPIs to deliver insights. The database is also made available to users to run their own data analysis.

The benefits of Data Analytics and Machine Learning are many for the end customers. Firstly, revenue can be increased by improving the throughput of the AGV system, i.e. moving more goods more quickly. Secondly, costly unexpected downtime is minimized by predictive maintenance. And finally, hyper-automating the configuration of the system contributes to reduced installation time.

Long time AI experience

Kollmorgen has been in the AI business for longer than most companies. The concept of AGVs has always been about teaching robots to solve complex task without human supervision. This is AI in its classical sense. For example, the route optimization that coordinates the AGVs is based on the A* algorithm, which has been a staple of Artificial Intelligence for decades.

Kollmorgen’s programmers develop and implement the AI algorithm, giving the computer explicit, step-by-step, instructions on how it should think. It this kind of AI that is behind our success. Be it disrupting the flexibility of AGVs by pioneering the laser navigation technology in the 1990s, or be it to safely handle a fleet of over 100 vehicles at a single site in the 2000s, AI continues to be the backbone of the technology we offer today.

The increased buzz around Artificial Intelligence in recent years has very much been focused on visual perception. The reason for this is not the progress in the theory of Artificial Intelligence per se, but has more to do with improvements in the processing power of computers. This has enabled the use of complex machine learning models in real world applications, such as object detection. From a mobile robot (AGV) perspective, having more ways to perceive and understand the environment allows the robot to make more intelligent decisions. For example, Kollmorgen uses machine learning in the form of neural networks to detect humans and estimate their pose, so that the robot can autonomously determine which way to drive to best avoid the human.

Machine learning is also an important part of data analytics, for example when building statistical models to understand what is normal and abnormal in the daily operations of a facility, or when predicting the remaining lifespan of an AGV component.

Creating a positive circle

Machine learning essentially rests on two pillars: automation and data. Since the two amplify each other, this combination is self-perpetuating. More automation yields more data, and more data powers more competent machine learning models, which in turn enables more automation. This offers an intuitive approach to artificial intelligence, where you can start with a low degree of automation, focusing on simple problems with clear boundaries. At the same time, you are collecting data, enabling more challenging applications. In this manner, the user gets the chance to gradually entrust the AI with increased responsibility as it learns. The increasing degree of automation means that more and more decisions are taken by the machines, saving time and resources.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…