Skip to main content
blog | AGV performance: a deep-dive into neural networks |
|
2 minute read

AGV performance: a deep-dive into neural networks

Machine Learning, Neural Networks – big terms in modern logistics, but what do they actually mean? What we need is an expert to tell us. Paul Hamblin, editor of Logistics Business magazine, meets one.

AGV and mobile robotics specialist Kollmorgen measures the performance and behaviour of AGV systems, both on a system level and on board individual AGVs. It collects information on motor drives, laser scanners, localisation, traffic, and obstacle interference, thus finding trends and patterns which help it to improve products and system configurations.

Highs and lows in productivity or daily utilisation trends might be measured, and the data used to optimise routes, increase throughput and calculate smarter resource utilisation. To the end-user, this translates into lower costs and higher revenue. The collected data can also give important clues to external processes that might disturb AGV performance. For example, pedestrians getting in the way of the AGVs, or manual forklifts driving in areas originally planned primarily for the AGVs.

How does it do all this, though? Samuel Alexandersson, Manager Product Management AGVs at Kollmorgen is our patient guide.

“An artificial neural network is a computational model that is loosely based on the structure of the human brain,” he begins. “Our brain cells, or neurons, are connected by an intricate network of nerves along which electrochemical signals travel. Simplified, we can say that if the weighted of input signals are strong enough, the neuron will fire, and the signal will continue on to the next set of cells the neuron is connected to.

“In this manner, the structure of the connections between all the different neurons in our brain will determine how a signal is propagated, and when we learn new things, what is really happening inside our brain, is that the connections are restructured.

“In an artificial neural network, the signals are digital instead of electrochemical, and the strengths of the connections are stored in weights. Initially, these weights will have random value, meaning when we feed an input to the network, it will just output random nonsense. But in the same way we humans learn from experience, we can let the model learn from experience in the form of data.

“Each datapoint will be an input and an expected output, so these pairs are examples to learn from. Using these so called Machine Learning algorithms to gradually adjust the weights, will bring the output from the model closer and closer to the expected output, so that it can learn to make predictions.

“For example, if we are to teach a machine to see the difference between a cat and a dog, we need to construct a dataset with images (inputs), where each image has a label indicating if it is a cat or a dog (the correct outputs). After training the neural network on the dataset, we may feed it with a new image, and even though this image has never been seen by the network before, it will tell us if it is a cat or a dog.”

Can he offer examples of how insights can be generated from data in a logistics context?

“Designing an AGV system can be a complex task that requires a lot of skill and experience,” he replies. “When designing the road network for example, there can be tens of thousands of individual road stretches that need to be configured correctly. Of course, it is easy to make a mistake and often such mistakes are not discovered until you run the system in a simulation.

“Therefore, we are currently developing tools that can analyze the road network directly, so that the user gets more immediate feedback. In internal AB-tests, we saw a 5x improvement in time it took users to find the root cause in a faulty configuration.

“A more anecdotal indication of the impact we can have with a data-driven approach, is a support case where something that an engineer had been debugging for several hours with conventional methods were resolved within 10 minutes using a prototype that automatically analyses the configuration data.”

So there we have it – as always, it’s all about cats and dogs.

Author: Paul Hamblin, Logistics Business Magazine

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…