Skip to main content
blog | Optimizing Robotic Arm Actuators for Articulated Motion |
|
2 minute read

Robotic arm actuators for articulated motion

The demand for high-precision robotics within the manufacturing, material handling, medical and aerospace sectors is accelerating. From surgical robots performing delicate incisions to industrial arms welding chassis on an assembly line, the room for error is effectively zero.

At the heart of these applications lies articulated motion—multi-axis movement that mimics the complex kinematics of the human arm but with vastly superior strength and repeatability. Achieving this level of articulation creates a considerable engineering challenge.

It’s not merely a matter of calculating trajectories from Point A to Point B. Designing robotic arm actuators requires rigorous control of torque, precise management of thermal dynamics, and the assurance of absolute repeatability under varying loads. The challenge becomes balancing all these problems simultaneously.

Why a System-Level Approach is Required  

Actuator performance is rarely the result of a single component. It is the outcome of system-level design, where motor density, transmission mechanics, and thermal management work together. Decisions in one layer can cascade through all the others.

The physics of articulated motion makes this especially pronounced. In a multi-axis robotic arm, multiple degrees of freedom are coupled together. Rotary joints, and sometimes linear axes, must continuously coordinate to place and orient the end effector. Any small design changes can ripple through the system, shifting torque-speed demand across the chain.

This is why robotic joints push for high torque density, compact packaging and peak acceleration capability. Performance must remain stable and responsive across a wide workspace and operating conditions. These interdependencies are also why actuator design decisions can’t be optimized independently.  

Instead, design requires continuous iterations. Because the actuator operates within an electromechanical system, every decision affects overall performance. Motor performance drives gearbox requirements, which in turn dictate your thermal management strategy. In humanoid and collaborative robotics applications, aesthetic and design considerations also increasingly influence joint form factor decisions, requiring teams to balance appearance with performance.

At Regal Rexnord, this interconnectivity is where we start. Effective robotic actuator design means engineering the full drivetrain as a cohesive unit versus optimizing components in sequence.

Finding the Right Form Factor and Architecture

Before selecting a motor type, engineers must define the shape of the available space. How much room does the joint allow? What is the geometry of that space? Does the application require a motor that is thin and long, or flat and wide with a larger outer diameter? Does cable routing require a hollow shaft? These spatial constraints define the actuator architecture before any other decision is made.

Robotic joints impose strict spatial constraints that influence motor selection, transmission layout, and integration. The right architecture is the one that solves the motion problem within the physical envelope available. 

Rotary with Precision Gearing

Rotary architectures dominate articulated robotic arms because they deliver high torque within a compact joint envelope. Precision gearing enables torque multiplication but introduces tradeoffs in backlash, stiffness, and efficiency that directly affect positioning accuracy and control response.

Direct Drive

Direct drive is used when stiffness and responsiveness take priority. Eliminating the gearbox removes backlash and improves control response, while enabling highly compact actuator integration. The tradeoff is that the motor must generate more torque directly, without the mechanical advantage of gearing. This increases demands for torque density, thermal management and continuous output capabilities. Note that "direct drive" can mean truly gearless, or it can describe a frameless motor that is directly embedded but still coupled to a gearbox.

Linear Actuation

Linear actuation applies where motion must be translated rather than rotated. For example, lifting axes, internal linkages like those used in leg extensions, or pulley-driven systems applied in humanoid hands. Ball screws and similar mechanisms provide high force and rigidity, though lower mechanical ratios mean inertia matching plays a larger role in system performance.

Frameless Integration

Frameless motors are selected when packaging and integration drive the design. Embedding the motor directly into the joint structure increases torque density and reduces overall size by eliminating duplicate housing and coupling components. This approach shifts responsibility for alignment, thermal paths and mechanical tolerances to the system level. While it can feel intimidating at first, the right assembly guidance and housing tolerance recommendations can make frameless integration far more accessible. And as robotic arm volumes scale, frameless motors that can meet demand while also proving portfolio depth for a wide range of joint configurations are increasingly essential.

Compact and Miniature Designs

Miniaturized actuators are used where weight and space are tightly constrained, such as in end effectors and hands. These designs must balance reduced size with torque output and heat dissipation. However, they often limit continuous performance if thermal management is not carefully addressed.

Torque and Motion Requirements

In robotic applications, torque is typically the primary constraint. It determines whether a joint can accelerate, decelerate and hold position under load. Inertia plays a supporting role, influencing the smoothness and curve of motion. But in most robotic systems with high-ratio gearboxes, sheer torque dominates sizing decisions.

The distinction matters for application context. High-speed industrial robots like sorting arms on a fast-moving production line experience significant acceleration forces and require careful inertia management alongside torque capacity. Surgical or precision systems, by contrast, may hold a position for most of an operation. In that case, continuous holding torque and long-term positional stability matter far more than dynamic response.

Designing for either environment requires a system-level approach. Increasing payload or reach raises torque requirements at upstream joints. Gear ratios influence both responsiveness and heat generation. Because these relationships are tightly coupled, iteration is continuous. Having robust calculation tools that account for all parameters simultaneously makes that iteration manageable.

Transmission and Precision Gearing

Transmission design is where performance gains are won or lost in robotic actuators. A precise motor paired with a compliant or poorly matched transmission will introduce oscillation at the end effector, eroding the accuracy and repeatability that the rest of the system was designed to deliver. The motion chain is only as strong as its most compromised link.

For rotary joints, the transmission must handle high dynamic loads during rapid acceleration and deceleration. High-stiffness gearing is necessary to transmit torque without introducing elasticity that degrades positioning accuracy. Tight tolerances and preload strategies also help minimize backlash and maintain control response throughout the duty cycle. For applications requiring linear motion, ball screws provide efficient conversion of rotary energy to linear force with high rigidity. The precision of the ball screw determines the smoothness and accuracy of the movement.

Material selection in gearing and ball screw components directly affects static and dynamic load capacity. Changes in hardness, alloy composition and surface coating can improve shock resistance and increase the amount of force the system can withstand. Selecting materials with compatible thermal properties can also help maintain clearances and prevent backlash from increasing as the system heats up. All of which helps extend service life.  

The benefits of these customizations can compound over time. The right material choice can extend operational life, which matters significantly in high-duty robotic applications. In longer lifecycle programs, Regal Rexnord offers deeper customization when standard configurations aren't sufficient.

Thermal Management and Heat Control

Heat generation is one of the primary limits on continuous actuator performance. This is because heat generated by the motor affects continuous torque capability, mechanical stability and system efficiency. As components heat up, they expand. Because different materials expand at different rates, the clearances set at room temperature will shift as the actuator reaches operating temperature. If those clearances close completely, the mechanism can seize or experience excessive friction, leading to motor burnout. If they widen, efficiency and mechanical stability can degrade over time.

Motor efficiency is your line of thermal defense. At Regal Rexnord, our motors are designed to perform at temperature without excessive heat generation. That’s because motors that run cool protect positioning tolerances, extend lubrication life and reduce the risk of thermal-related failure across the duty cycle.

Beyond the motor, a heat dissipation strategy depends on how hard the system works. Passive cooling, or utilizing the thermal mass of the housing and fin design, is sufficient for many applications. However, high-duty industrial robots often require active cooling methods, such as forced air or liquid cooling, to stay within safe operating limits. In either case, integrating thermal sensors gives control systems visibility into temperature trends before they become failures, turning reactive maintenance into predictive.

Reliability and Lifecycle Performance

Robotic actuators are typically sealed systems. There is no scheduled re-lubrication, as there might be for large industrial equipment. The lubrication in the system at commissioning needs to last, which means thermal management is about protecting the conditions that keep lubrication effective throughout the system's lifetime.

Lubrication is one of the first things to degrade under high temperatures. When viscosity drops too far, the hydrodynamic film protecting gear and bearing surfaces breaks down, accelerating wear. When it's too high during cold startup, the motor works harder against fluid resistance, reducing efficiency. Managing the temperature environment is, in large part, managing lubrication health.

Over a system's operational life, backlash, thermal effects and lubrication degradation interact. Small clearances become larger. Wear accumulates, and thermal cycling introduces material fatigue. Designing for reliability means accounting for how the system behaves from startup through the end of its duty life.

Material selection, sealing, thermal design and component tolerances all contribute to whether a system holds its performance window over time.

Partnering to Synthesize the System

Optimizing robotic arm actuators is an exercise in interconnectivity. A powerful, high-torque motor is ineffective if paired with a transmission that introduces excessive compliance. A precise gear set will fail prematurely without proper lubrication and thermal management. The entire electromechanical drivetrain must be engineered as a cohesive unit, and actuator requirements evolve as programs move from prototype to production in ways that make the supplier relationship as important as the design itself.

Regal Rexnord brings a family of brands spanning motors, gearing, ball screws, mechanical components, and precision products like brakes and bearings with the engineering depth to understand how they interact. That breadth enables a holistic view of a customer's problem, and our experience across design, materials and global manufacturing help identify gaps early. This matters even more than ever as robotic programs scale. From individual components to integrated robotic arm actuator designs, we can co-engineer solutions or deliver within defined parameters to meet your requirements.

To explore how Regal Rexnord can support your robotic actuator program from concept through production, consult with our engineering team.

Consult an Expert

Frameless Motors

Discover Kollmorgen's frameless motor range, designed for easy integration into your application, enhancing performance, efficiency and reliable motion solutions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
Designing Field Robots for Harsh and Unpredictable Environments

Designing Field Robots for Harsh and Unpredictable Environments >

This session explores how innovative technologies from Kollmorgen and Regal Rexnord’s broad portfolio of motion control technologies can help engineers meet the rigorous demands of field robotics.
Motion Control Principles for Scalable Humanoid Robotics

Motion Control Principles for Scalable Humanoid Robotics >

As humanoid robotics gain momentum across industries—from logistics and manufacturing to healthcare and public safety—the demand for precise, efficient, and scalable motion control solutions is accelerating. Engineers face complex challenges in…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…