Skip to main content
blog | Hangcha Intelligent Empowers Intelligent Ceramic Production: New Pearl Group's Transformation Through Advanced Manufacturing |
|
2 minute read

Hangcha Intelligent Empowers Intelligent Ceramic Production: New Pearl Group's Transformation Through Advanced Manufacturing

In the ever-evolving landscape of manufacturing, innovation stands as the cornerstone of progress. New Pearl Group, a pioneering force in the ceramics industry, has taken a significant leap forward by embracing intelligent production techniques. Collaborating with Kollmorgen's cutting-edge navigation system and integrating Hangcha Intelligent's 3-ton omnidirectional Automated Guided Vehicles (AGVs), New Pearl Group in partnership with Hangcha Intelligent has revolutionized its production line to meet the demands of the modern world.

Ceramic production is an intricate process that demands precision, durability, and efficiency. However, the production environment presents numerous challenges. The ceramics industry is characterized by high temperatures and dust-laden surroundings, posing a unique set of challenges for manufacturing processes. Furthermore, ceramic products themselves are often delicate and weighty, necessitating careful handling and transport to ensure product integrity and safety.

Hangcha Intelligent Empowers Intelligent Ceramic Production: New Pearl Group's Transformation Through Advanced Manufacturing

The integration of Hangcha Intelligent's 3-ton omnidirectional AGVs, equipped with Kollmorgen's advanced navigation system, has proven to be a game-changer for New Pearl Group in the ceramic production. These AGVs are engineered to withstand the harsh conditions of ceramic production, ensuring seamless operations even in high-temperature and dusty environments. Their robust construction and high load-bearing capacity make them ideal for handling the fragile yet weighty ceramic products.

One of the most noteworthy advantages of this integration is the realization of continuous 24-hour production cycles. The combination of Hangcha Intelligent's AGVs and Kollmorgen's navigation system has enabled New Pearl Group's production lines to operate round the clock. This not only meets the demands of a competitive market but also enhances overall productivity.

A key benefit of employing AGVs lies in their capacity to reduce reliance on manual labor, subsequently boosting operational efficiency. By automating material transport and handling, New Pearl Group has streamlined its processes and reduced the risk of human errors. The AGVs efficiently navigate the challenging production environment, carrying heavy loads and fragile ceramic products with precision and care.

Hangcha Intelligent Empowers Intelligent Ceramic Production: New Pearl Group's Transformation Through Advanced Manufacturing

Moreover, the utilization of forklift AGVs has significantly curbed the incidence of cargo losses. Fragile ceramic items are transported securely and without compromising their integrity. This has had a cascading effect on warehouse management. The AGVs have achieved a remarkable 100% shelf usage rate, optimizing storage capacity within the production workshop. This not only reduces wastage but also enhances overall resource utilization.

In conclusion, New Pearl Group's adoption of intelligent manufacturing techniques, in collaboration with Kollmorgen and Hangcha Intelligent, has ushered in a new era for ceramic production. The challenges posed by the harsh production environment and delicate products have been met with ingenious solutions. The integration of AGVs and advanced software systems, powered by Hangcha Intelligent, has not only elevated production efficiency but has also fortified product safety and integrity. New Pearl Group's journey in partnership with Hangcha Intelligent serves as an inspiring testament to the transformative power of innovation in manufacturing. As the industry evolves, such groundbreaking approaches are sure to reshape traditional paradigms and pave the way for a smarter, more efficient future.

For more information visit this link.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.