Skip to main content
blog | Can You Integrate a Superior Motor into Your Existing Food and Beverage Production Line? |
|
2 minute read

Every machine designer wants to deliver the best possible performance. Especially in today’s food and beverage industry, the pressure for optimum throughput and quality means that every OEM is striving to engineer new systems that are the best of the best.

For existing systems, realities are that machines operating in the field don’t always perform as well as intended. For example, motors can fail prematurely if they are not properly designed to withstand frequent washdown cycles. Supplies may be hard to come by without an overly long lead time. Or, to keep up with the competition, manufacturers may simply wish to boost performance without a major re-engineering effort.

For both new and existing machines, being locked in to a particular motion supplier can feel like an insurmountable obstacle. Food and beverage systems require considerable time, effort and expense to develop. Choosing a supplier is a big commitment—and once the choice is made, starting over with a different partner is rarely feasible.

But what if you could choose a dependable source of more reliable motors without abandoning your entire motion control platform and going back to the drawing board?

With Kollmorgen motors, you can.

Our AKM and AKMH Series motors can operate with drives from leading PLC brand’s automation system in any food and beverage production environment. We can match these motors to the specific voltage/encoder/format requirements of your production system, with a correct fit to your installation footprint and with significantly better reliability and performance.

For example, for all standard 240 VAC and 480 VAC drives, we offer hygienic, washdown and food grade motors featuring 18-bit absolute single-turn or multi-turn digital encoders , 4096 revolutions, using the Hiperface DSL protocol, as well as several other standard feedback device options. These motors can operate with leading PLC brand’s drives, but if you should have any question about your particular integration, we encourage you to contact us to discuss your options.

Which Kollmorgen motors should you choose, and why?

In high-moisture environments and for the most rigorous of washdown regimens, our Stainless Steel AKMH Series combines IP69K construction, corrosion-resistant materials, and a patented pressure-equalization system to eliminate contamination by water and corrosive chemicals—the main cause of motor failure in washdown environments. These are servo motors you can expect to last the life of your machine.

For low-moisture environments with less-frequent washdown requirements, you still need a reliable supply of high-performance motors configured to your specifications. Our AKM Washdown and Food Grade servo motors meet the need with a protective 2-K coating, IP67-rated seals, stainless steel hardware, food-grade greases, and reliable delivery in the quantities you need, without excessive lead times, wherever in the world you operate.

There is no motion partner more responsive to your supply requirements and more committed to consistent quality than Kollmorgen. Ready to lock in performance without partner limitations? Talk with a Kollmorgen engineer today to configure a motor that's the best fit for your existing platform. Let’s discover all your food and beverage machine is capable of.

Consult an Expert

AKMA Servo Motors

The lightweight AKMA servo motor is designed for harsh environments like food and beverage processing, and delivers performance and reliability.
Learn More

Stainless Steel Food Grade AKMH Series

The AKMH Series is built to withstand the most rigorous of washdown regimens. The combination of the AKMH’s IP69K construction and corrosion resistant materials make for a servo motor that will last the life of your machine.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

cost-optimized motion control

Reliable, Cost-Optimized Motion Control for Food Processing Washdown Applications >

Join this live webinar to discover how Kollmorgen Essentials™ Servo Drives (KED) paired with AKMA washdown motors and AKMH hygienic stainless‑steel motors deliver high‑performance, washdown‑ready motion across food contact, splash‑zone, and non‑food…
English, UK
Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments

Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments >

Kollmorgen Corporation, a global leader in motion control and automation solutions, has expanded the application range of its Kollmorgen Essentials™ Servo Drive (KED) to include hygienic and washdown environments.

Enhancing Washdown Motor Performance with a Unified, Cost-Optimized Motion Control System >

In this webinar, you’ll discover how the Kollmorgen Essentials™ Servo Drive (KED), combined with IP69K-rated AKMA anodized aluminum and AKMH stainless-steel servo motors, deliver reliable, high-performance motion at a value-driven price.

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging >

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure…

How can food packaging machine builders meet stricter food safety rules without sacrificing OEE? >

Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…

From the Factory to the Farm: Unleashing the Power of Kollmorgen's Servo Motor Technology >

As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.

Kollmorgen introduces the AKMA servo motor to meet the demands of medium- to heavy-washdown applications >

Kollmorgen extends its highly regarded AKM servo motor portfolio with a new high performance servo motor that delivers durability, cleanability and versatility.
AKMA Servo Motor in washdown

Bringing Performance and Reliability to Harsh Environments with Lightweight AKMA Motors >

Learn how lightweight Kollmorgen AKMA servo motors deliver durability, cleanability and performance in medium and heavy washdown applications.
Sleeger Success Story

Food Processor Meets Hygienic Requirements >

A company that specializes in creating cutting, placing and packaging machines looked to Kollmorgen for an innovative motor design. See how the AKMH motor met the strictest hygienic requirements and integrated with a third-party drive.