AKD PDMM Hardware Revision Number
| Hardware Revision | Firmware Version | Date | Remarks |
|---|---|---|---|
| DB | 1.6 | 30.05.2012 | Starting version, incl. AKD HWR D and PDMM HWR B |
| EB | 1.13.0 and later | 2014-12 | Hardware revision for export classification traceability purposes |
Kollmorgen Support Network
A component of the Kollmorgen Automation Suite, the AKD PDMM™ Drive Resident Controller combines an integrated AKD servo drive with an embedded motion controller that can control up to 64 axes, and the full automation capability of Kollmorgen Automation Suite™ in a single, compact package.
| Current Drive Firmware Version | 1.21.00.000 |
| Current Runtime Firmware Version | 3.07 |
| Firmware Release Date | 12/9/2021 |
| Firmware History & Downloads | KAS Associated Firmware by Release |
| Current Hardware Revision | EB |
| Part Number Scheme | Open the PDF |
| KAS IDE Compatibility | v2.9 and later |
| Current KAS IDE Version | v3.07 |
| Release Date | 12/9/2021 |
| Model | Processor |
|---|---|
| AKD-M0xxxx-MCEC | 800 MHz single-core |
| AKD-M0xxxx-M1EC | 1.2 GHz single-core |
| Digital/analog I/Os | MultiFieldbus | Position output (encoder emulation) | Software interfaces | MultiFeedback |
|---|---|---|---|---|
|
|
See Protocols Supported by AKD Drives for more products |
|
| KAS v4.05 Software is now available! | English | ||
| Retrofit KAS EtherCAT Backups with AKD2G Firmware | English | ||
| KAS v4.01 Software is now available!! | English | ||
| Trade Compliance | English | ||
| AKT and AKT2G Remote I/O Comparison | English | ||
| KVB HMI - Displaying Bitwise Variables in KVB / AKI2G | English | ||
| AKD2G Gantry Mode with KAS Controller | English | ||
| Getting Started with PxMM UDP Communications - using Packet Sender | English | ||
| MLFB_HomeFindHomeInput with additional features | English |
Although Windows displays this message and the limited functionality icon for the drive connection, your PC can communicate fully with the drive. This message and the icon are normal for an AKD to PC connection.

This is because you are using the Windows classic theme. To get a white background you must change the theme that Windows is using.
To change the theme go to the Control Panel, select Display, select the Themes tab, and choose a new theme, such as "Windows XP".
See Device not Shown in the Workbench Help for a detailed discussion of this problem.
If you are communicating through the Ethernet port at connector X11, you might not see your drive in the connect window for any of the following reasons:
In most cases, firmware is downloaded using WorkBench without setting the hardware into a specific “download” state. If you need to download firmware, but are unable to connect to WorkBench, use the procedure described in Forcing the drive into firmware download mode in the Workbench help.
Autotuning of your application delivered unexpected results while tuning the current feed forward value. Please deactivate "Tune Acceleration FF" in the Workbench Performance Servo Tuner screen and restart the tuning.

Up to 500 s depending on the active current. See page Foldback Times.
5 seconds with Ipeak. Smaller currents can be sustained for longer periods. See Foldback Times.
There are two ways to find out about what parameter is behind a text box in Workbench.