Search Articles
| Jog ModeValid for S300, S400, S600, S700 | English | |
| Delay of Enable SignalValid for S300, S700 | English | |
| Analog Position SetpointValid for S400, S600 The analog input can be used for the setting of the position from firmware version 3.10. The function is similar to a master/slave effect. | English | |
| Speed adjustment with external position feedbackValid for S300, S400, S600, S700 | English | |
| Memory CardValid for S700 | English | |
| Reaction to fault situations S300-S700Valid for S300, S700 Depending on the current trouble, faults are managed differently (different error levels): | English | |
| Setup of Acceleration Profile TablesValid for S300, S400, S600, S700 Create table with Excel, normalize current / position values | English | |
| Analog Torque LoopValid for S400, S600 | English | |
| Safe Reduced SpeedValid for S400, S600 | English |
Accueil >
Base de connaissances >
FAQ >
Téléchargements >