Setup of Acceleration Profile Tables
Valid for S300, S400, S600, S700
Create table with Excel, normalize current / position values

Save as DOS *.CSV file and edit (commata)
Split several tables with ";". Maximum 16 tables are allowed, maximum 8,000 points are allowed.

Convert table in the DOS screen with calclk_52b.exe
Download this tool from page Tools.

Download the file with the "Drive Can Download Tool"

Testing of motion task profile tables
Check the table with LOOKUP as a trigger signal.
Example:
Tables 0 to 3 are predefined Acceleration profile tables. Table 4 is the new table.

Trigger! LOOKUP user defined + Trigger Level 4

Create motion tasks with the table
Total motion time = Acceleration ramp + Deceleration ramp.

Oscilloscope
If the speed is not zero at the beginning or at the end of the movement, then the motor axis will jerk.

Home >
Knowledge Base >
FAQs >
Downloads >