Skip to main content

Kollmorgen Support Network

DBL / DBK

Discontinued

The synchronous servomotors of the series DBL/DBK are brushless three-phase motors for high quality servo-applications. This is a Service product: the DBL/.DBK servo motors are not available for new applications but replacement motors are available.

Connection Method

MotorFeedbackPower
DBL1Cable, Speedtec-ReadyCable, Speedtec-Ready
DBL2, DBL3, DBL4, DBL5, DBL6, DBKSpeedtec-ReadySpeedtec-Ready
DBL7, DBL8Speedtec-ReadyTerminal box

Matching mating connectors for Speedtec-Ready: M23 threaded connectors or Speedtec connectors.

Further Information

Trade Compliance English
Bethany…
Servomotoren German
…
Rundlauf, Koaxialität, Planlauf German
…
NEMA Baugröße German
…
Motordaten Legende German
…
Normen und Richtlinien German
…
Leistungsreduzierung German
…
DBL - DBK Motoren mit Micron Getriebe German
…
Rastmoment German
…
What commutation offset do Kollmorgen motors have?

DBL / DBK with Encoder

Feedback has no defined commutation offset. The commutation offset is determined with the help of the servo amplifier and stored in the encoder memory.

AKM with Hiperface encoder

Encoder is installed arbitrarily. The commutation offset is determined with the aid of the servo amplifier and stored in the encoder memory.

AKM with BiSS encoder

Encoder is installed arbitrarily. Commutation offset is set to zero electronically.

AKM with EnDat encoder

Commutation offset is mechanically set to zero.

What is the maximum value for motor temperature sensor (PTC)?

That depends on the servo amplifier that is used.

S300 5.0 kOhm
S400 2.0 kOhm
S600 1.6 kOhm
S700 5.0 kOhm
Which parameters affect synchronism of the servo motors?

See page Synchronism.

What motor is described by motor number 19071?

That is an AKM72M (480V). A list of all motor numbers can be found in the Motor Database, available from the Downloads page.

What is meant by four quadrant operation?
Is it possible to test a servomotor by connecting it directly to the main supply?

No, this is forbidden. Connecting a motor directly to the main supply will destroy the motor. Refer to the chapter "Use as directed" in the instructions manual.

Is it possible to suppress the motor cogging?

Yes, for the Servostar line it is possible with S300 and S700. See page Cogging Suppression for details. For AKD drive family the feature is available in firmware version 1.15 See Cogging Compensation for details.

I want to replace a 6SM servomotor with an AKM. What motor type is required?
I am experiencing positioning errors with AKM1 motors. What can I do?

Low rotor inertia is the source for this problem, ironless linear motors show a similar behavior.

Solution for drives with S300/S700 servo amplifiers:

Increase the bandwidth of the current control loop with the Smith Predictor (FILTMODE = 2). Refer to page Tuning: Delay Time Compensation with Smith Predictor.