AKD-C/N
The AKD-C Power Supply and AKD-N drives lie at the core of a decentralized drive system. Up to 16 AKD-N drives can be connected to one AKD-C central power supply. Hybrid cables are used to connect the AKD-C to the drives and to daisy-chain the drives. For more specific information about the individual components, see the AKD-C and AKD-N topics.
| Current Firmware Version | 1.20.00.001 |
| Firmware Release Date | December 2020 |
| Current Hardware Revision (AKD-N) | B |
| Current Hardware Revision (AKD-C) | A |
| Hardware Release Date | 01/01/2014 |
| Part Number Scheme | AKD-N (PDF) AKD-C (PDF) |
| See the WorkBench article for details about the software used to configure and manage the drives. | |
| Components | |
|---|---|
| AKD-C | Central Power Supply |
| AKD-N | Decentralized Servo Drive |
Blue Boxes: All components in the blue box are products delivered by Kollmorgen. For detailed information click to the product or use the table below for navigation.
Gray Boxes: Elements in the gray area are components which have to be added by the machine builder.

| AKD-C | AKD-C Power Supply |
|---|---|
| AKD-N | AKD-N Drive |
| AKD-CN-Coupling | Connector interface for cabinet wall (in process) |
| AKD-M | AKD PDMM Drive |
| AKM | AKM Motor |
| AKMH | AKMH Motor |
| AKI | Operating Console |
| AKT | KAS Input and Output Terminals |
| BAR/BAS/BAFP | Brake Resistor |
| Cx Cables | Configured CC/CM/CF cables for connection of the components, refer to the cable part number scheme |
| DDL | Linear motors (on request) |
| ENCP | Ethernet cables |
| Gearhead | Micron Gearheads |
| Heatsink Kit | optional accessory for AKD-N |
| KAS-IDE | KAS System Setup Tool |
| KBM | KBM Motor |
| KCM | KCM Capacitor Module |
| Redi Mount | Adapters to mount Micron Gearheads to AKM motors |
| Workbench | AKD Setup Tool |
| Trade Compliance | English | ||
| KAS v3.07 is now available!! | English | ||
| What is a Subnet Mask? | English | ||
| Resolving Servo Feedback Choices | English | ||
| Compartilhamento do Barramento DC entre Drives AKD e AKD-C | Portuguese, Brazil | ||
| AKD and EtherCAT CSV Mode | English | ||
| FAQ Seiten | German | ||
| Clearing an AKD-C Power Supply Fault from a PxMM Application Program | English | ||
| AKD EtherCAT Max Torque Scaling - Object 6072 | German |
Although Windows displays this message and the limited functionality icon for the drive connection, your PC can communicate fully with the drive. This message and the icon are normal for an AKD to PC connection.

This is because you are using the Windows classic theme. To get a white background you must change the theme that Windows is using.
To change the theme go to the Control Panel, select Display, select the Themes tab, and choose a new theme, such as "Windows XP".
See Device not Shown in the Workbench Help for a detailed discussion of this problem.
If you are communicating through the Ethernet port at connector X11, you might not see your drive in the connect window for any of the following reasons:
- Poor cable connection. Make certain you have a good connection between your computer and the drive by checking to see if you see a blinking light next to the connector (at each end).
- Improper rotary switch setting. Make certain that the S1 and S2 rotary switches on the front of the drive are set to 0 (bottom position), unless you are attempting a point to point connection and your computer is set up to connect in this manner.
- Conflict with another device that is networked to your computer (including your wireless connection). In some cases, turning off your wireless card will fix this. You can turn your wireless card back on after you establish communication with the AKD).
- Improper TCP/IP settings. Make certain that the TCP/IP settings in the network port that you are communicating through are working properly.
In most cases, firmware is downloaded using WorkBench without setting the hardware into a specific “download” state. If you need to download firmware, but are unable to connect to WorkBench, use the procedure described in Forcing the drive into firmware download mode in the Workbench help.
Autotuning of your application delivered unexpected results while tuning the current feed forward value. Please deactivate "Tune Acceleration FF" in the Workbench Performance Servo Tuner screen and restart the tuning.

Up to 500 s depending on the active current. See page Foldback Times.
5 seconds with Ipeak. Smaller currents can be sustained for longer periods. See Foldback Times.
There are two ways to find out about what parameter is behind a text box in Workbench.
- Right click on the text box and select Parameter Info from the menu. A popup appears next to the window selected. Note if you clicked the Help, you get taken to the page in the help system. Pressing F1 also does the same.
- Click the “Tell me more about this topic” link at the top of each page.
Home >
Knowledge Base >
FAQs >
Downloads >