Skip to main content

Kollmorgen Support Network

Search Articles

KAS 2.10: Fieldbus Editor Does Not Display All Supported Network TypesThe fieldbus editor may not display all the supported network types. The network types that are not displayed are ... English
Changing variable values over Telnet to AKD BASIC programThis application note details how to pass values via Workbench terminal, Hyper terminal, or some other method ( i.e. high level programming language, etc. ) via Telnet commands. English
AKD Profinet Drive Supported ProtocolsThe Service Port on all AKD drive models supports Modbus TCP, EXCEPT the ProfiNet model (AKD-P-NxPN).  While the AKD-P-NxPN can communicate Telnet and ProfiNet at the same time, Modbus TCP support was NOT added to this model. English
AKD RSLogix AOI AKD_Two_Axis_Move blockThis block performs a linear X-Y move with two axis.  It is not “true” coordinated motion.  It calculates two motion task for X and Y axis to perform a simultaneous move that results in the correct linear point to point move.  Each axis moves independent of each other but the motio English
AKD EtherNet/IP AKD_Start_MotionTask & AKD_Set_Motion_Task BlockThis is a simple RSlogix 5000 AOI block that starts an existing Motion Task that is already existing in the AKD drive.  There is also a block to create MT at any MT number. English
Registration with PLCopen Example ProjectThe attached KAS project contains a Registration example used on a real machine. It is a two axis program that uses PLCopen motion functions. English
Create a New Template in KVBTo create a a new template in KVB do the following: English
Handling Multiturn Overflow in KAS for Non Modulo AxisA multiturn encoder delivers feedback position in 32 bits format. The lower 20 bits provides single turn information and the higher 12 bits provides the multiturn information. English
PCMM - New KAS Controller!The PCMM (Programmable Controller Multi-Axis Master) is a PDMM (Programmable Drive Multi-Axis Master) without an internally integrated AKD drive.  It shares the same electronic hardware, connectors, and signals as the PDMM.  It has the same features, functionality, and performance as the… English