AKD EtherNet/IP AKD_Start_MotionTask & AKD_Set_Motion_Task Block
This is a simple RSlogix 5000 AOI block that starts an existing Motion Task that is already existing in the AKD drive. There is also a block to create MT at any MT number.
7/10/2019-updated the AKD_Set_MotionTask AOI from the previous v1.0 to v2.0. Changed MT.ACC, MT.DEC, MT.V, MT.P instances to 32 bit ( 4 byte ) instances. This allows MT.P to be set to negative values via the AKD_Set_MotionTask AOI.
7/19/2019-AKD_Start_Motion_Task 2.2
Changed IP status to be based on Profile In Progress it instead of not on target position.
Added N.C. contact for No Profile In Progress status in addition to the existing on
target position status to unlatch the Start_Block bit of the control word.
This fixed the issue of the AOI running successfully once but then being immediately done and PC complete
before every executing the subsequent move.
Home >
Knowledge Base >
FAQs >
Downloads >