AKM Packaging & Transport
Packaging
The Motors are delivered in cardboard packing with Instapak® foam cushion. You can return the plastic portion to the supplier for disposal. Technical Information from Instapak® supplier for disposal in Europe.
Transport
![]() |
We recommend the transport tool ZPZM 120/292 for moving the AKM7 and AKM8 motors (>20kg). Suspended Unit ZPMZ 120/292 consists of a beam, suspended to the crane hook and two double-run chain suspenders. ZMZ 60/8 suspenders (the number depends on the motor type, are part of delivery of the motor). The motor may be borne on two or four runs of the chain suspender. For a description see the AKM PDF Archive for the "AKM Transport Instruction Manual". |
Home >
Knowledge Base >
FAQs >
Downloads >