Skip to main content
Success Story | 2 minute read

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

Rbot9 invented the first industrial cable robot: the ROCAP. Suspended by twelve motor-driven cables, the overhead platform travels above the factory floor. Designed for extra-large work envelopes, ROCAP spans up to 900 m², lifts payloads up to 250 kg, and supports a wide range of end effectors. Anchored to the facility’s existing structure, it eliminates the need for bulky gantries and rails, offering a faster and more flexible alternative to traditional automation systems.

Challenge

Rail-based automation systems are inflexible and require substantial installation work. Ground-based robots compete for floor space. Large-scale gantry systems are complex and costly. Rbot9 sought to overcome these challenges with an architecture based on 12 independent, robotically controlled cables, each actuated by a motor/gearbox assembly.

Each motor must deliver high torque at high speeds while maintaining a compact form factor. In addition, motion systems must be able to brake vertical loads precisely and reliably to ensure safety and performance. And due to the large dynamic forces involved, the system must incorporate effective energy management to prevent regenerative energy from causing overvoltage conditions on the servo drives.

Solution

Each of the 12 cables are coordinated to precisely position a centralized platform with an end effector that is capable of moving a payload of up to 250 kg at a top speed up to 1 m/s. To achieve these performance characteristics, Rbot9 selected Kollmorgen AKM2G servo motors paired with AKD servo drives.

AKM2G motors provide industry-leading torque density, delivering on average 30% more continuous torque than other, comparably sized servo motors. This allows OEMs to substantially increase machine performance without increasing the motor footprint, or conversely to achieve a desired torque specification while using a smaller motor.

Additionally, AKM2G motors are available with an integrated holding brake option. The brake works in conjunction with the integrated functional safety features optionally available on AKD servo drives. In particular, Rbot9 uses the Safe Torque Off (STO) feature to meet compliance requirements for safely managing vertical loads, without the need for external safety components. The AKD drive also supports an optional regen resistor to dissipate excess energy while braking.

Together, these features contribute to a more modular, responsive, cost-effective robotic platform than would otherwise be possible.

Results

Rbot9 upgraded its cable robot design to Kollmorgen AKM2G motors and AKD drives in March 2024, and the robot has been productive in the field since fall of that year. Compared to previous designs, Kollmorgen technology has more than tripled the speed of operation, from 0.2 m/s to 1 m/s, while maintaining the full 250 kg payload and ensuring vertical-load safety.

Integrating the motion system is also significantly smoother and faster thanks to the Kollmorgen ecosystem and the support of Kollmorgen’s local distributor, Electromate, which provided valuable assistance with configuration and testing.

Rbot9’s first customer, a fish-processing facility that uses the system for automated cleaning of conveyor systems, is now considering an expansion project incorporating additional Rbot9 systems in their plant.

See RBOT9 ROCAP in action

“The Kollmorgen drives have been a key enabler in helping us unlock higher speeds without compromising on torque or safety. Combined with excellent support from Electromate, this collaboration has allowed us to push our cable robot platform to the next level.” — Frederic Vachon, Founder and CEO, Rbot9

Power cable robots application image

Power cable robot stats

Download as PDF

AKME Series Servo Motors

AKME Series is built on the AKM platform and designed for use in Zone 2 and Zone 22 environments with ATEX and IECEx global certification.
Learn More

Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever

Learn how an off-the-shelf motion system powered the fastest puzzle cube-solving robot. Speed, precision and synchronized multi-axis motion explained.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When should you convert from a stepper motor to a servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
Automatic Pick and Place machine installing components on circuit board

How mechatronics design improves motion system performance >

Discover how mechatronics design boosts motion system performance by integrating servo systems and control for faster commissioning and integrated motion.
Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.