Skip to main content
Success Story | 2 minute read

Robotic arm application with frameless BLDC motor

In industrial automation, robots are typically designed for a specific task or application. This makes it challenging to adapt systems when requirements change. RobCo, a Munich-based startup, set out to change this with the world’s first modular industrial robot kit that supports 1- to 8-axis configurations.

RobCo’s innovative and end-to-end robotic solutions enable customers to assemble, reassemble, and extend robots as needs evolve. For small-to medium-sized businesses where production changes weekly, this adaptability is a real game-changer. By combining interchangeable arms and joints, RobCo transforms a single component family into an endless number of robotic solutions.

However, as adoption of its modular robot platform increased, RobCo required a dependable motion solution and partner that could perform reliably and scale with its business.

“TBM2G-powered joints deliver low torque ripple, which is important for smooth, slow motion in many applications such as surface grinding. We greatly appreciated Kollmorgen’s co-engineering support throughout all phases of the project to make it a success.”
—Paul Marold, Co-Founder & Head of Customer Value Engineering

Challenge

By offering one joint that addresses multiple robot challenges, RobCo’s modular approach allows customers to optimize for their specific reach, payload and workspace requirements. This flexibility, however, places higher demands on the motion components at the heart of each joint.

A single joint design must perform consistently across a wide range of torque, speed and load conditions while remaining compact enough for embedded robotic designs. It is essential that motion remains smooth and predictable, particularly during slow, controlled movements. Motors must integrate seamlessly with standard mechanical interfaces to preserve modularity and avoid the need for custom designs for each new configuration. Any compromise in size, performance or integration reduces the advantages and benefits of a modular robot platform.

Solution

To meet these requirements, RobCo partnered with Kollmorgen to standardize its robot joint designs using the TBM™2G frameless BLDC (brushless DC) servo motors. Available in seven widely used frame sizes and multiple stack lengths, the TBM2G helped RobCo’s robots deliver high torque and speed in an ultra-compact design.

The motor’s frameless architecture allowed for compact joints with short axial lengths and high torque density. Standardized motor dimensions enabled direct integration with off-the-shelf strain wave gearing, supporting compact rotary joints for industrial robot applications. Finally, the TBM2G’s large inner diameter supported RobCo’s integrated hollow-channel design for cables and hoses to pass through the joint cleanly.

Beyond the hardware, Kollmorgen supported RobCo through a collaborative engineering process focused on long-term stability and manufacturability. Motor performance was validated through analytical simulations and detailed operational data, while application support assisted RobCo’s production team in transitioning to the new motor technology.

Kollmorgen TBM2G Frameless Motor w/ Reflection

Results

With the TBM2G motors in place, RobCo expanded what customers could achieve with a single modular robot system. Using the same core joint architecture, customers can now configure robots with a reach up to 2,100 mm and a payload up to 13 kg, or a reach up to 1,200 mm with a payload up to 40 kg. Existing robots can also be reconfigured for new applications by swapping arms or joints, thereby extending the system lifespan and maximizing flexibility without redesigning the entire robot.

The ultra-compact joints also deliver high torque density and low torque ripple for precise, smooth motion. This is especially important in controlled, slow-speed tasks, such as surface grinding, where motion quality directly affects the finished result.

Since the partnership began, RobCo has steadily scaled production to meet growing market demand and expanded its international presence, all while maintaining reliable performance and preserving the modular flexibility at the core of its platform.

Download as PDF

Incorporating Frameless Motors Into an Environmentally Resilient Design

Daily washdowns, deep-sea submersion, high radiation, high vacuum, hazardous atmospheres: When a housed servo motor can’t provide the protection you need in a compact form factor, consider embedding a frameless servo motor. Read this white paper to learn how.

Learn More

Achieving Ultimate Motion Precision Using Frameless Servo Motors

Frameless motors aren’t just for robotic joints. Compact actuators, sensor system gimbals, submersible propulsion systems and other applications benefit from direct drive precision and compact design. Learn how to directly embed a frameless motor in your mechanism.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
Designing Field Robots for Harsh and Unpredictable Environments

Designing Field Robots for Harsh and Unpredictable Environments >

This session explores how innovative technologies from Kollmorgen and Regal Rexnord’s broad portfolio of motion control technologies can help engineers meet the rigorous demands of field robotics.
Motion Control Principles for Scalable Humanoid Robotics

Motion Control Principles for Scalable Humanoid Robotics >

As humanoid robotics gain momentum across industries—from logistics and manufacturing to healthcare and public safety—the demand for precise, efficient, and scalable motion control solutions is accelerating. Engineers face complex challenges in…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…