Skip to main content
blog | How mechatronics design improves motion system performance |
|
2 minute read

Automatic Pick and Place machine installing components on circuit board

Machines are becoming faster, more precise and more interconnected. As complexity evolves, so does how we measure performance. Instead of focusing on isolated parts, performance now depends on how the entire motion system behaves under real conditions, including speed, load, variability and synchronization.

This shift is what makes a mechatronic approach valuable. It means designing systems where mechanical, electrical and control disciplines work together from the beginning. With this lens, engineers move beyond isolated optimization and build motion systems that perform consistently from commissioning through operation.

What mechatronics design means for modern motion systems

At its core, mechatronics design brings together mechanical structures, electrical components and control engineering into a single system. The motor, drive, controller and software act as a single organism. Each discipline influences how the machine moves, but performance depends on how they interact.

Mechanical design defines stiffness, inertia and load dynamics. Electrical systems determine how power is delivered and converted. Control engineering governs how motion is commanded and stabilized. When combined, their interaction is the primary driver of performance.

In applications such as packaging systems or precision assembly, these interactions determine whether motion remains stable at speed or becomes sensitive to variation. Designing for interaction from the outset is key.

The limits of component-level design

Traditional motion system design often focuses on optimizing individual components. This might mean selecting a higher-torque motor, a faster drive or a more rigid structure. These decisions matter, but they don’t guarantee system-level performance.

In many cases, optimizing one element can bring about new challenges elsewhere. For example, a high-performance servo system can still underperform if mechanical compliance introduces vibration, and a precisely machined structure can lose accuracy if control loops are not properly tuned.

As motion systems become more complex, especially in multi-axis applications, these interactions become more visible. Performance depends less on peak specifications and more on how well the system maintains motion quality across all axes and operating conditions.

Designing integrated motion systems

An integrated motion system brings motors, drives, feedback and control into a coordinated architecture—moving from selecting components to shaping system behavior.

With this approach, axes are engineered to work together. They are synchronized to follow precise motion paths, respond to disturbances, and remain in alignment under dynamic loads. Feedback and control are also applied system-wide for a consistent response.

Control engineering allows this behavior. It defines how the system reacts to commands and disturbances and how motion stays stable within the limits of system dynamics and control bandwidth. Modern control systems regularly monitor system performance to pinpoint early signs of variation and adjust in real time.

This level of integration reduces the need to manually align and tune individual components. Instead, engineers can design and optimize the system as a whole for faster commissioning and more predictable performance.

From manual input to automated accuracy

For many years, setting up a servo system meant doing everything manually. Engineers entered motor parameters into the drive by hand, referenced lookup tables, and hoped nothing was mistyped. A misplaced decimal point could cause a motor to overheat or damage itself. Small errors meant poor performance, instability, or unexpected behavior before the machine ever ran a real cycle.

Modern systems address this directly. Kollmorgen's SFD-M smart feedback device stores motor data in the feedback device itself, enabling automatic configuration between motor and drive—loading the correct parameters for torque, current and speed control without slow or error-prone manual entry. The system performs as intended from the first test move.

This is the first stage of mechatronic integration in practice: enabling key elements to cooperate automatically. It shifts engineering focus from configuration to machine dynamics.

Beyond setup, modern drives are designed to operate across multiple industrial networks by default. OEMs often have existing automation environments and communication protocols they're committed to. Protocol-agnostic drives remove that barrier, while fully integrated environments like the Kollmorgen Automation Suite (KAS) bring motion control, PLC logic, safety and visualization into a single workspace. Essentially, mechanical intent and digital control are in one place.

Validating motion performance across the machine lifecycle

Designing an integrated motion system is only part of the challenge. Engineers must also ensure that performance holds under real conditions before the machine is built, during commissioning, and throughout operation and maintenance.

Digital twin and simulation technology help address this early. By combining mechanical models with drive characteristics and control behavior, engineers can model system response under different conditions. This helps identify tradeoffs early and reduces the need for repeated physical testing during development. While virtual tools don’t replace physical testing, they do help improve system understanding before deployment. 

Once operational, a unified system also simplifies maintenance and fault tracing. When components from multiple vendors are stitched together, identifying the source of a fault becomes time-consuming and uncertain. A unified system removes that ambiguity. Issues are easier to trace and resolve, and upgrades or replacements are more straightforward because new components can be validated without redesigning the surrounding system.

This matters especially in globalized engineering environments where a machine may be designed in one region, assembled in another and serviced in a third. Integrated platforms and shared digital environments help maintain performance and consistency across those boundaries, ensuring the design behaves the same no matter where it's built or operated.

Driving motion performance in the real world

Even with the right design and validation approach, performance is ultimately proven in application. Understanding how motion systems behave in specific use cases—from packaging lines to robotics to precision assembly—helps ensure that design decisions translate into real-world performance.

Ultimately, the value of mechatronics is in what happens when all elements come together. Machines built as unified systems are easier to develop, tune and maintain. They run more smoothly, adapt more readily to future needs, and deliver greater long-term reliability.

Contact us today to learn more about applying a mechatronic approach to the design of your motion systems.

Consult an Expert

AKME Series Servo Motors

AKME Series is built on the AKM platform and designed for use in Zone 2 and Zone 22 environments with ATEX and IECEx global certification.
Learn More

AKMA Servo Motors

The lightweight AKMA servo motor is designed for harsh environments like food and beverage processing, and delivers performance and reliability.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When should you convert from a stepper motor to a servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple

Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple >

Introducing Kollmorgen’s AKME servo motors—ATEX/IECEx certified and engineered for compact, versatile performance in hazardous environments where choices have been limited—until now.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK
Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español)

Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español) >

Descubre cómo Kollmorgen Essentials ofrece control de movimiento de alta precisión y fiabilidad comprobada, ahora más rápido de configurar, más fácil de integrar y más rentable de escalar.
Español
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
Which Servo Position Feedback Device Is Right for Your Application?

Which Servo Position Feedback Device Is Right for Your Application?  >

Choose the right feedback device for your application. Learn how to achieve maximum performance, efficiency and value with a multi-turn absolute rotary encoder.