Skip to main content
Success Story | 2 minute read

Explosion-proof technology helps create  a safety shield for heavy-duty AGVs

Chemical, painting, polishing and other specialized production environments require equipment that meets strict standards for safety and stability. As factory automation accelerates and manufacturing capabilities expand, there is an increasing demand for heavy-duty automated guided vehicles (AGVs) capable of operating in hazardous areas. Recognizing the opportunity in this rapidly developing market, a prominent leader in the explosion-proof equipment industry launched a project to develop a heavy-duty AGV that can safely transport materials across a variety of hazardous locations, while potentially exposed to ignitable gases or dusts. 

Challenge

For this AGV project, the manufacturer wanted to develop a heavy-duty AGV with a load capacity of 2-3 tons and ATEX/IECEx certification for use in Zone 2 and Zone 22 areas where explosive gases and dusts may occasionally be present. At the same time, the goal was to achieve mass production in a relatively short period of several months. To reach these ambitious product-development targets, the manufacturer needed to address several technical challenges:

  • How to choose a suitable servo drive system to meet the operational requirements of heavy-duty AGVs.
  • How to optimize the drive parameters to ensure low energy consumption and high rigidity while carrying heavy loads.
  • How to ensure effective management and collaboration as the project progressed and the size of the technical team grew.

Solution

Based on the customer’s application requirements, Kollmorgen provided a motion control solution of AKME hazardous-location motors with AKD servo drives, plus a full range of technical support to ensure that the AGV meets performance expectations. The AKME series builds on the proven performance of the AKM servo motor platform, adding enhanced design features to achieve ATEX (EN 60079) and IECEx certification for use in explosive atmospheres such as gas Zone 2 and dust Zone 22 hazardous locations. The AKME servo motors are also supplied with a shaft seal as standard, giving the motor an IP64 protection rating against the ingress of liquids and dusts.

The AKD servo drive has very high responsiveness, with a current loop bandwidth up to 4000Hz, speed loop bandwidth up to 1000Hz, position loop bandwidth up to 250Hz, and a data refresh rate up to 1.5MHz. The drive is optimally matched to the AKME servo motor to enable powerful, accurate control of the AGV.

Through the close collaboration between Kollmorgen and the customer’s teams, the heavy-duty, hazardous location AGV fully met the strict requirements for ATEX Zone 2 and Zone 22 certification, payload capacity and the travel speed requirements.

Results

The project also achieved aggressive goals for mass production at scale in response to rapidly growing market demands. It took less than six months for the AGV to go from prototype to launch with local certification. The AGV is now globally certified and widely praised for its exceptional performance in heavy duty applications across both standard and hazardous-location environments.

Download as PDF

The Scalable Humanoid Robot

A successful prototype may prove a concept, but the actuator architecture determines if it can scale. This gap is why many humanoid programs stall when transitioning from working prototype to manufacturable product.

Learn More

Navigating Hazardous Locations: How to Select ATEX & UL Certified Motors

A complete compliance guide for aligning ATEX and UL requirements with performance to optimize servo motor selection for HazLoc environments.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scalable Humanoid

The Scalable Humanoid Robot >

A successful prototype may prove a concept, but the actuator architecture determines if it can scale. This gap is why many humanoid programs stall when transitioning from working prototype to manufacturable product.
Advanced stainless steel processing equipment found in pharmaceutical or biopharmaceutical manufacturing facilities

Hazardous location servo motors for freeze dryer applications >

Discover why​​ explosion-proof servo motion is key to safe lyophilizer hatch control in pharmaceutical hazardous gas Zone 2 and dust Zone 22 locations.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Hazardous location facility

Navigating Hazardous Locations: How to Select ATEX & UL Certified Motors >

A complete compliance guide for aligning ATEX and UL requirements with performance to optimize servo motor selection for HazLoc environments.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Which Motor Should You Choose for Your Hazardous Location Application?

AKME vs. Goldline: Which Motor Should You Choose for Your Hazardous Location Application?  >

The new AKME Series for hazardous locations brings ATEX and IECEx certifications, unprecedented compactness and versatility. Compare AKME against Goldline EB.
Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple

Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple >

Introducing Kollmorgen’s AKME servo motors—ATEX/IECEx certified and engineered for compact, versatile performance in hazardous environments where choices have been limited—until now.

AKME Series Servo Motor Catalog >

AKME servo motors are built on the proven performance of the AKM servo motor platform, with additional design features to achieve ATEX and IECEx certification for operation in gas Zone 2 and dust Zone 22 hazardous locations. To suit a wide range of…