Stepper systems can be efficient, powerful and quiet — but only if you get it right. When specifying stepper motors and drives, here are 5 common mistakes to avoid and 5 best practices to implement, speeding your development of a successful machine.
To win in the competitive eVTOL market, you need a source for optimized motion solutions throughout the aircraft. Learn why Regal Rexnord Aerospace Solutions is your ideal partner.
When most engineers think of a brushless DC servo motor, they’re likely to visualize a housing with a flange to accept mounting bolts, connectors to accept power and data cables, and a rotor shaft that couples to the load. That’s the most common…
When it comes to exoskeletons, motion design and motor selection are make-or-break steps in the engineering process. Here we explore key considerations and insights for success.
With rapid growth in the worldwide market for missiles, and demand for ever more innovative capabilities, engineers need rapid access to highly specialized motion systems, produced in reliable quantities. Learn how to greatly accelerate design and…
No two projects are the same, and it’s important to be able to provide a modular solution that can be adapted to suit the customers’ requirements. Learn how Heli created specialized high-reach AGVs equipped with Kollmorgen technology to meet their…
Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…
In factories and warehouses, we have these clever machines known as Automated Guided Vehicles (AGVs) and Autonomous Mobile Robots (AMRs). They're changing the way we manage materials by doing tasks on their own, making manufacturing and warehousing…
Humanoid robots are projected to become a $6+ billion opportunity within the next 10 to 15 years.1 Many labs, research entities and startup companies have taken notice, and are rushing to develop concepts and prototypes ahead of the competition. But…
In a short time, humanoid robots have progressed from science fiction to a $6+ billion opportunity. Learn how to succeed in this exponentially growing market by solving motion challenges far beyond the requirements of conventional industrial robots.
With the urgent need to replace fossil fuels, repeated shocks to the oil & gas supply chain, and technical advancements combined with lower costs for electrical systems, the drive toward electrification is transforming the way we live and work.
Electric motors generate heat under normal operating conditions and have the potential to generate a spark if a motor coil fails. Excessive motor case temperatures or a spark that is not properly contained can cause an explosion or ignite a fire in…
A servo drive is an electronic device that is part of a closed loop system, producing current and voltage to rotate a servo motor. The closed loop system includes the servo drive, servo motor and feedback device, and is commanded from an analog or…
There are several considerations when selecting a servo motor for a specific application, such as the required speed, torque or force, motion profile, available physical envelope, and environmental factors. This means that the chosen motor solution…
A servo motor is an electromechanical device that produces torque and velocity based on the supplied current and voltage. A servo motor works as part of a closed loop system providing torque and velocity as commanded from a servo controller utilizing…
Most of the AKD drive’s parameters have a 32bit data size, but some parameters have a 64bit data size. Modbus communication on the AKD drive uses registers of a 16bit data size. So for a 64bit parameter, it takes four registers to send…
Electric motors are used in machines and processes all around us. You can find them in factories, automobiles, airplanes, robots and even your favorite DVD vending machine. Regardless of the application, managing heat dissipation is a…
An alternative to customizing a servo motor is utilizing a frameless motor and integrating directly into the machine itself. Learn more in our new blog post!
From the surface of Mars to the depths of the ocean, from the core of the earth to the core of the human body, Kollmorgen motion systems take on the most extreme environments.
Companies working toward the consumer market have long invested in and understood the value of user experience (UX) design. A good user experience is a key differentiator in today's market, and by aligning your company to ensure that your customers…
Kollmorgen Automation is part of Kollmorgen, which in turn belongs to the NASDAQ-listed Altra Industrial Motion group. The company develops and sells products and services related to automation solutions for applications that include warehousing and…
The need for flexible automation for material handling has now moved from being an interesting technology project for enthusiasts to conscious decisions made in the board room of Fortune 500 companies as well as the private owned, small sized…
Many of us do not truly understand or appreciate the underlying foundations for how and why mankind has achieved such enormous success and prosperity. More commonly, we are taught about problems with the world and the challenges that we will face in…
Successful CSR (Corporate Social Responsibility) is about action. An often overlooked action to improve CSR is industrial automation with AGVs (Automated Guided Vehicles). Well-known for their quick efficiency gains in industries and warehouses, AGVs…
Automated guided vehicles work repetitively, never get tired and are easy for staff to get used to. An excellent way forward for any company that wants to improve safety at work – and as a bonus increase their productivity.
Automated guided vehicles minimize the need for manual labor in dirty, dangerous and demanding environments. In most conditions, they are resistant to or can be shielded against everything from magnetism and radiation to temperature changes, dirt and…
Trending in the automation world these days is the merging of the collaborative robot and the AGV, creating a mobile Cobot with the navigational capabilities of today’s AGV’s. This opens new opportunities in warehouse logistics that improves the…
Automation is not only about efficiency. It is also about safety. Moving things in a controlled way in manufacturing plants and warehouses contributes significantly to fewer injuries and less damage to goods, pallets and racks. Zero accidents is a…
The trend is clear: more and more companies, large and small, are turning to solutions involving Automated Guided Vehicles (AGVs). The development of new vehicle types and technology break-throughs in fields like AI leads to more intelligence in AGV…