Skip to main content
blog | How to Select a Servo Motor |
|
2 minute read

There are several considerations when selecting a servo motor for a specific application, such as the required speed, torque or force, motion profile, available physical envelope, and environmental factors. This means that the chosen motor solution must produce the load torque and speed requirements, fit in the available space, and perform as required under the subjected environmental conditions of the application.

A servo motor is part of a total mechanism that provides motion to a load – to move it, machine it, lift it, inspect it, etc. The servo motor is the muscle that provides the necessary torque, force, and speed (required load point) to perform a given function. The fastest and most reliable way to determine these needs is with a motor sizing tool that calculates the load points required by a motor and analyzes information about the load, transmission elements, and motion profile to select a motor from the motor database that matches the load parameters. As the initial load points are determined, the sizing tool checks for the optimum solution and narrows the motor choices based on the required torque, speed, inertial ratio, and associated margins acquired from the motor ratings.

A servo motor’s physical size is mostly determined by its continuous torque producing capability with a tradeoff between motor diameter and motor length. A longer motor with a small diameter can have the same torque rating as a shorter, larger diameter motor. Another way of achieving the power requirements is by using a smaller motor and multiplying torque through a gearhead or applying alternative technologies - such as a flatter, direct drive servo motor, a frameless or kit motor, or a linear motor. Each of these technologies has varying forms that can address specific space requirements.

Environmental considerations can affect the motor choice in several ways. In most applications, the motor’s operating ambient temperature remains below a motor’s rating (typically 40°C). The motors themselves generate a prescribed amount of heat (based on the continuous rating designated by the manufacturer) which is represented by a temperature rise of the windings and a maximum coil temperature. For example, if a motor that is rated to produce 10 lbft of torque in a 40°C ambient with a 130°C temperature rise and a maximum coil temperature of 170°C is placed in a 50°C ambient environment, the maximum coil temperature of 170°C will be exceeded when the motor is operated at the 10 lbft rating continuously. In this case, the motor’s continuous torque would be reduced unless a larger motor is selected. More exotic environments may require customized solutions, including alternate materials, special sealing arrangements, or other modifications. The motor performance can be adversely affected in extreme conditions, such as outer space, high altitude, and even submersible environments.

Know your application requirements but not the necessary torque and speed? Use Kollmorgen's Motioneering tool to size your project and find motor and drive pairings that best fit your needs.

Consult an Expert

AKME Series Servo Motors

AKME Series is built on the AKM platform and designed for use in Zone 2 and Zone 22 environments with ATEX and IECEx global certification.
Learn More

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When should you convert from a stepper motor to a servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
Automatic Pick and Place machine installing components on circuit board

How mechatronics design improves motion system performance >

Discover how mechatronics design boosts motion system performance by integrating servo systems and control for faster commissioning and integrated motion.
manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple

Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple >

Introducing Kollmorgen’s AKME servo motors—ATEX/IECEx certified and engineered for compact, versatile performance in hazardous environments where choices have been limited—until now.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK
Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español)

Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español) >

Descubre cómo Kollmorgen Essentials ofrece control de movimiento de alta precisión y fiabilidad comprobada, ahora más rápido de configurar, más fácil de integrar y más rentable de escalar.
Español
Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever

Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever  >

Learn how an off-the-shelf motion system powered the fastest puzzle cube-solving robot. Speed, precision and synchronized multi-axis motion explained.