Skip to main content
blog | Key Tips on Dealing with 64-bit data on Modbus Communications Devices that only Support 32-bit data |
|
2 minute read

AKD servo driveMost of the AKD drive's parameters have a 32-bit data size, but some parameters have a 64-bit data size. Modbus communication on the AKD drive uses registers of a 16-bit data size. So for a 64-bit parameter, it takes four registers to send the data over Modbus.

There are many devices, including PLC's, HMI's, and PC programs that do not handle a 64-bit data size. So what can be done to read and write 64-bit values when working with Modbus and a device that only supports 32-bit values?

There are two approaches to limiting a 64-bit value to 32 bits. One is to simply not use the two upper registers. The other method is to use the Modbus addresses specifically made to be 32-bit versions of the 64-bit parameters.

In many cases, the position scaling can be set in such a way that the position values, such as PL.FB, will not exceed 32 bits. For example, if you set the position scaling to 10000 counts per motor revolution, then it would take 429,496 motor revolutions to fill up the 32-bit position value. If you never move the motor that far, then you will never use the upper two registers of the 64-bit position value.

For any parameter that may have a negative value, the sign bit is contained in the upper most 16-bit register. So if you choose to limit a 64-bit parameter to a 32-bit value by not using the upper two registers, then you will be eliminating the sign bit and the value will not be allowed to be negative. Just like you can use only the lower two registers of a 64-bit parameter to make it a 32-bit value, you can also just use the lowest 16-bit register of any parameter, whether 64-bit or 32-bit. There are many AKD parameters with values that never exceed 16 bits and always have a positive value.

The order of the Modbus registers is important. For the AKD drive, the Modbus address number is the address of the upper most register. Again with PL.FB, the address is 588, which is the address of the most significant register of that parameter. Register 591 is the lowest, or least significant, register. So keep in mind which registers you want to read or write to when using only a portion of the parameter data size. Registers 590 and 591 are the lower two registers (32 bits) of PL.FB. Modbus

The second method is to use the Modbus addresses that are remapped from 64-bit to 32-bit. For example, Modbus address 588 is for PL.FB and is four Modbus registers (588, 589, 590, and 591). Modbus address 2072 is for PL.FB as a 32bit data size, including the sign bit. It is two Modbus registers.

Consult an Expert

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

AKD Servo Drive

AKD® Series is a proven perfomer, supporting the largest customer installed base, and offers:

  • Industry leading motion control loops
  • Extensive motor feedback and drive fieldbus support including EtherCAT, EtherNet/IP, Profinet RT, etc.
  • Plug-and-play with Kollmorgen motors
  • WorkBench GUI, acclaimed for customer experience and usability
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Introducing the latest update to SafeMotion monitor firmware - SMM 3

Kollmorgen advances linear motor safety and performance with SafeMotion Monitor firmware upgrade >

The latest SafeMotion Monitor™ firmware (SMM 3.0) expands functional safety for linear motors with EnDat 2.2 safe feedback support and SIL 3 compliance.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK
Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español)

Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español) >

Descubre cómo Kollmorgen Essentials ofrece control de movimiento de alta precisión y fiabilidad comprobada, ahora más rápido de configurar, más fácil de integrar y más rentable de escalar.
Español
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments >

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor…