Skip to main content
blog | 5 Mistakes to Avoid When Specifying a Stepper System |
|
2 minute read

5 Mistakes to Avoid When Specifying a Stepper System

We all make mistakes — even machine engineers. Almost always, a mistake is an opportunity to learn and grow. Or, as the great Irish author Samuel Beckett put it, “Try again. Fail again. Fail better.”

But in order to engineer a market-worthy product, this cycle of failing better must ultimately lead to success. Of course, the best scenario is to get it right the first time. We’re here to help.

Once you have evaluated your choice of motion technologies and decided to use a stepper system, you’ll need to choose the optimum motor and drive for your application requirements. This is one area where it can be all too easy to make mistakes that affect your development time and costs.

So let’s look at the five most common mistakes that engineers make when specifying and working with stepper motors and drives, the problems that can result, and how you can avoid them. We’ll also list five best practices for making the right choice.

Mistake 1 — Believing that a motor will deliver its speed and torque ratings when matched with any stepper drive

With servo motors, you’re probably already aware that the rated torque, stall torque and speed are all specified under ideal conditions. The values you obtain in actual use depend as much on the pairing of drive and motor as on the available voltage and current. The same principle applies to stepper motors and drives.

The most reliable way to ensure you’ll get the performance you require in a stepper motor is to model its performance when matched with the available voltage and current of a particular drive that has the features you need. Generating a performance curve (speed-torque curve) for the matched motor and drive provides the most reliable reference.

Kollmorgen’s online Stepper Optimizer tool makes this process easy. Begin by choosing a motor that physically fits your application, then modify the available voltage and current to produce a torque/speed curve for your drive. Or, alternatively, identify your required torque/speed or basic motion profile, then let the tool automatically find the best solution that fits your application requirements.

Keep in mind that a motor’s stall torque is not an indication of the torque it can generate while moving — especially during accelerations and decelerations, where higher torque is required. Using the Stepper Optimizer to choose a system based on your application’s actual dynamic requirements can help you avoid this mistake.

Mistake 2 — Specifying a microstepping drive for the wrong reasons

If you’re looking for the greatest possible control over velocity and position, a servo system is likely a better choice for your application than a stepper. But it may be tempting to specify a stepper motor and microstepping drive instead, thinking you can achieve comparable accuracy without necessarily requiring feedback-based control. This can be a mistake.

Microstepping was developed to allow motors to overcome the effects of noise and vibration at the low-end resonant regions or even to run continuously within these low-end regions. The drive divides the 1.8º step angle into as many as 250 microsteps, but these individual pulses may not be uniform. The motor’s position and velocity are not necessarily constant down to the microstep level. While a microstepping drive does deliver higher resolution than a standard stepper drive, this doesn’t necessarily guarantee an increase in accuracy.

Instead, a primary benefit of microstepping is reduction of vibration, noise and ringing at low motor speeds. This brings us to another potential mistake — expecting a microstepping drive to mitigate all resonance issues. In addition to low speeds, stepper motors can also exhibit a resonance period around the mid-speed range. Microstepping will not help with this issue. Instead, choosing a drive with anti-resonant algorithms is the best way to handle these resonances.

Mistake 3: Undersizing or oversizing the motor

Undersizing a stepper motor will at best cause excessive heat, unsatisfactory acceleration and deceleration, and generally poor performance. At worst, the motor will lose pulses, position improperly, or stall altogether under heavy loading or high acceleration and deceleration.

Oversizing the motor will cause it to generate more audible noise as well as higher EMI/RFI noise. It may also mean higher costs for the motor and drive as well as wasted panel space and a machine that’s larger and heavier than necessary.

Kollmorgen’s Stepper Optimizer tool can help you avoid these basic mistakes, leading you to the motor that best fits your application’s size and performance requirements.

Mistake 4: Mismatching load-to-motor inertia

The old rules of servo system inertia matching no longer apply. But for stepper systems, it’s still as important as ever to consider the load-to-motor inertia since these systems are typically open-loop. Even when adding an encoder to create a closed-loop stepper system, an inertia mismatch cannot be much more than one order of magnitude (10:1) without causing the motor to lose pulses, misposition the load, draw excessive current or even stall.

Mistake 5: Failing to account for the machine’s inherent frequencies

Engineers should understand the machine’s characteristic frequency (omega-natural), as well as its anti-resonant frequency, and avoid commanded speeds that are within the system’s natural frequency range. A microstepping drive with anti-resonant circuitry will help greatly with this, but the machine will still ring at certain motor speeds if care is not taken to select a motor and drive combination that can perform outside of these resonances. Choosing the wrong stepper for such an application can result in a noisy machine that vibrates at certain speeds and performs unreliably.

5 best practices for making the right choice the first time

  1. Make sure you understand your machine’s mechanical limitations and requirements such as mechanical resonant frequency, mechanical bandwidth, load inertia​ (ideally ≤ 10:1), static and dynamic friction, and so on. This is true for any equipment that incorporates motion, no matter how precise.​
  2. Use a sizing program such as Kollmorgen’s Stepper Optimizer to properly size your system based on reliable speed-torque performance curves.
  3. Select a drive that matches the available bus voltage and has the desired features, and select a motor that offers the required performance curve — outside the machine’s resonant frequency — when matched with the drive.
  4. Don’t force steppers into the role of performing high-speed or high-precision motions where a servo may provide a better results. Just like steppers, servos have come down in price over the years and are much easier to apply.
  5. Get collaborative engineering help. Kollmorgen offers the industry’s highest-performing motors and drives, but we’re much more than just a supplier. Our mission is to help your application be the best it can be. Get in touch with our motion experts, and get started optimizing your machine today.

FAQ

  • Q: What should I consider first when specifying a stepper system?

    A: When specifying a stepper system, the first step is understanding the application requirements, including load, speed, accuracy, and duty cycle. Many issues arise when a stepper system is selected based on motor size alone, without considering how the full system behaves under real operating conditions. A clear definition of performance needs helps avoid oversizing, inefficiency, or missed steps.

  • Q: Why is torque often misunderstood when specifying a stepper system?

    A: Torque ratings are frequently misinterpreted because holding torque is often confused with usable torque at speed. When specifying a stepper system, it’s important to evaluate torque across the entire speed range, not just at standstill. Ignoring this can result in poor acceleration, resonance issues, or unreliable motion.

  • Q: When should I consider alternatives to a traditional stepper system?

    A: If the application requires higher speeds, quieter operation, or closed-loop feedback, it may be worth reassessing whether a standard stepper system is the best fit. When specifying a stepper system, understanding its limits helps determine when hybrid or servo-based solutions may provide better long-term performance and efficiency.

Consult an Expert

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Expand Machine Capability with Programmable Stepper Drives  >

Discover the future of stepper drives. Join us as we explore advanced, software-programmable ​stepper ​solutions in this new online webinar.

Get Exact Positioning Without the Complexity with Stepper Motors >

If you’re looking for precise motion with easy setup, then stepper motors should be your first choice when building or upgrading a machine.
What You Need to Know When Selecting a Drive for Your Stepper Motor

What You Need to Know When Selecting a Drive for Your Stepper Motor >

To get the most out of your stepper motor, you need to pair it with the proper drive. There are three critical elements to keep in mind when making your selection: voltage, current and inductance. Each one plays an important part in a motor’s…

Why Does My Stepper Motor Get Hot? >

All electric motors heat up during operation, which is simply a product of passing current through a coil of wire. Electric motors use copper wire to form coils that are part of the electromagnetic circuit required to produce rotation. While copper…

The Big Debate – Stepper vs Servo >

What is the best motor technology to use in a motion control application? There are numerous technologies to create motion, from hydraulic to pneumatic or electromechanical. In the world of precision motion control, many machine designers face a…
Kollmorgen stepper motor

How to Select a Stepper Motor >

Knowing how to selct a stepper motor is critical for optimal performance. Use our speedy, dependable Stepper Optimizer tool for precise selection.

How Does a Stepper Motor Work? >

A stepper motor is a simple two phase brushless synchronous motor containing a segmented magnetized rotor and a stator consisting of a prescribed number of electromagnetic coils. When energized, these coils create north and south polls that push or…

Going Small - How Current Step Motor Technology Can Help You Reduce Machine Size >

As it turns out, "going small" is an effort that traces back to the first steppers ever manufactured. Released in 1952, the Sigma "Cyclonome 9" series, one of the first steppers ever designed, was the first standard offering of its kind. Motors had a…

That's One Small Step... 0.9 vs 1.8 Degree Step Angle >

There is a lot of discussion about the 1.8 degree step angle versus 0.9 degree step angle of industrial hybrid stepper motors.  Most stepper motors today have the standard step angle of 1.8 degrees, resulting in a 200 step per…