Skip to main content
blog | How Mobile Bots Made it to the Board Rooms |
|
2 minute read

The past decade, I have been fortunate to get to know the world of autonomous vehicles used for logistics and material handling worldwide.

When I started to work for Kollmorgen, the Automated Guided Vehicles (AGV) technology had been available for many decades and truly contributed to the success of many companies in the world. More often, the installations were driven by technology enthusiasts, or early adopters if you may, who wanted to be pioneers and saw AGV systems as a chance to try something new and different. In some cases, the systems installed in lengthy projects were way too complicated and the cost for implementing and maintain these systems were much higher than the value they brought to the chain they operated in. In the bad examples the leadership teams were not even aware what was tested at the shop floor but when budgets were exceeded and return on investment couldn’t be seen, the projects sure made their way to the board rooms in a very unpleasant way.

In my first role with the company, I got in contact with one of those systems. One of those lengthy complicated ones. Project plans where renewed, more investments were approved as that was the only way to get coverage for the sunken cost, it was said. The installation was finalized and in the final handover meeting, the project manager on the customer side said, “ It has been a long and winding road to get us here, but all in all, even with the extra investments from all included parties, the return on investment is less than 24 months”. They later ordered an extension of the installation and the AGV technology is now rolled out widely within their group.

The need for flexible automation for material handling has now moved from being an interesting technology project for enthusiasts to conscious decisions made in the board room of Fortune 500 companies as well as the private owned, small sized company. Why? one may ask. Because the business case is very reliable, and the savings can be predicted if you know what you do.

With a steady growth and a market need that is favorable, more innovators, investors and business developers show up. This leads to more companies, analyses and technology is seeing the light and it can sometimes be hard to distinguish what is real facts and what is marketing buzz.

One thing that is very important to remember, is that new functions like obstacle avoidance and other features, new sensors, Big Data, cloud-based services and 5G is only relevant and important if they in the end add value to a chain of operations. Innovations must always prove themselves valuable!

At Kollmorgen, we Enable Innovators to make the world a better place. Our strive is to combine the latest and greatest innovations with the experience we possess. By doing so, we can offer our strategic partners a very comprehensive toolbox that will enable them to build material handling solutions that are robust and reliable, as well as easy to work with and flexible. We call it NDC Solutions. Our commitment is to offer our partners the best technology there is so they can solve their material handling challenges. In our world, you may define them as AMR’s, AGV’s, Mobile Robots or Autonomous Transporters, but in the end the only important is that the solution provides value where they are installed. The technology you choose should deliver a favorable business case that makes the world a better place!

We are experiencing critical times and the effects of the coronavirus has already been seen and remains to be seen. It is a terrible pandemic that affects our behavior and the way we will live our lives in the future. One thing is for sure, we will come out on the other side and when we do, automation, material handling and logistics will lead the way to the new future.

Personally, for me and my team at Kollmorgen AGVs & Mobile Robots, health and safety are our highest priorities. We are doing our outmost to help our society fight the outbreak. Meanwhile, we are relentlessly working on bringing new innovative technology to NDC Solutions that will empower businesses with the next generation of automated logistic technology.

If you want to know more about NDC Solutions or how to become a strategic partner, just reach out to us!

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…