Skip to main content
blog | Kollmorgen Does Not Make Robots - We Move Yours |
|
2 minute read

Trending in the automation world these days is the merging of the collaborative robot and the AGV, creating a mobile Cobot with the navigational capabilities of today’s AGV’s.  This opens new opportunities in warehouse logistics that improves the entire supply chain.  With additional power demands created by this combination, innovative motor and drive solutions become paramount.

'MARS' demo at Pack Expo 2018Kollmorgen demonstrated this concept at PACKEXPO 2018 with the “MARS” Robot. MARS stands for Mobile and Robotic Arm Solution and shows how the world of mobile robots/AGVs and Collaborative Robots are starting to come together. AGV’s have a strong presence in smart warehousing applications and is starting to move out of the main aisle and into picking aisles, manufacturing cells and even in office spaces and out in the fields. Kollmorgen applied its core expertise in frameless motors, drives, and navigational controls to show just how we can help manufacturers build better robots and AGV’s.  

For mobile platforms and AGVs:  Kollmorgen (NDC) has the most versatile AGV controls platform available with the largest network of AGV partners globally.  The Kollmorgen platform offers 6 navigation options with a single controller - this means flexibility in how your AGV navigates.

For robots and cobots: Kollmorgen has an established track record for enabling robotic innovation with 100 years of experience, tens of thousands of motor designs and mobilizing hundreds of thousands of robot joints and robotic arms.  Our frameless technology is versatile and optimized for performance, enabling smaller, lighter and faster robots.  Our TBM and KBM platforms provide the foundational building blocks and can be optimized for the perfect performance and mechanical fit.

The Kollmorgen MARS robot demonstrates these two worlds coming together which includes an interactive demo of a robotic arm enabled by Kollmorgen Automated Guided Vehicle (AGV) software, hardware, and integrated frameless motion technology.

Kollmorgen does not make robots but our technology moves them.

For more application and product information, see Kollmorgen/Robotics or NDC Solutions.
 

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…