Skip to main content
press_release | Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis |
|
minute read

NDC Layout Assistant

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout quality, improving performance and shortening design and validation time while establishing a strong foundation for future AI-driven capabilities.

Simple insight for smarter layout decisions

Many organizations struggle with limited visibility into layout performance. Problems are often discovered late, fine-tuning the layout can require a lot of manual work, and it is unclear where changes will deliver the greatest benefit.

NDC Layout Assistant responds to these challenges by making layout performance transparent from the start, serving as a smart layout guide.

Immediate layout quality feedback

The tool delivers instant insight into potential layout issues, making it easier to identify which segments have the greatest optimization potential early in the design process. This enables faster improvements and higher design quality with fewer iterations.

Focus on what matters most

Performance is analyzed at segment level, allowing users to clearly see where inefficiencies occur—even in complex layouts. Segments with the highest optimization potential are highlighted, helping teams focus on the areas with the greatest impact.

Clear, actionable segment data

For each segment, NDC Layout Assistant provides essential metrics:

  • travel time
  • drive speed
  • optimization potential

Visual indicators help users spot segments with inefficient travel times or drive speeds, making it easier to identify where improvements are needed.

A more efficient design workflow

By reducing the time spent identifying issues and validating changes, NDC Layout Assistant supports a faster, more predictable workflow. Users    can prioritize improvements, shorten simulation cycles, and communicate results more effectively — leading to layouts that perform as intended, sooner.

Contact Kollmorgen

Automotive Manufacturing Logistics

Automotive manufacturing demands precision. AGVs ensure reliable material flow, reduce downtime, and improve efficiency—supporting just‑in‑time production while increasing accuracy and overall performance.
Learn More

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.

CVC700HW Datasheet >

The CVC700 vehicle controller is a first step toward a modular AGV system. It offers increased processing power and enhanced communication, using the same successful form factor and IP65 housing as the CVC600