Skip to main content
Success Story | 2 minute read

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully implemented Jungheinrich Automated Guided Vehicles (AGVs) with Kollmorgen technology and is the first terminal within DB Schenker land to use automated forklifts in terminal operation.

DB Schenker in Borås, Sweden, has successfully implemented Jungheinrich Automated Guided Vehicles (AGVs) with Kollmorgen technology. As a leading provider of land transports of both goods and parcels, this marks a significant milestone in the company’s automation of intralogistics.

Embedded Video

Fredrik Ottosson, Terminal & CoDi Manager at DB Schenker Land in Borås, highlights the challenges faced by the facility in efficiently moving goods within tight timeframes. "The main challenge on this site is to move a lot of goods in a very short time," says Ottosson. “We also have a target in cluster SE/DK Land to increase automation within our terminals. This is showing a good step forward in this direction”.

Recognizing the potential of AGV technology to enhance efficiency and streamline operations, DB Schenker chose Jungheinrich AGVs with Kollmorgen technology for their proven track record and tailored solutions. “We have six AGVs working in two shifts. They are running parcels to and from the sorting facility and preparing the operations for the new shift”, explains Fredrik Ottosson.

Jungheinrich, renowned for its intralogistics expertise, provided a comprehensive system design encompassing AGV vehicles equipped with Kollmorgen's automation kit. Bardia Emad, Head of Automation Units Nordic at Jungheinrich, emphasized the company's commitment to automation and the integration of their middleware, the Jungheinrich Logistics Interface, facilitating seamless operation control via tablets. "We are proud to work in this innovative way, and that this is one of the first automated forklifts in DB Schenker Land," remarked Bardia Emad, highlighting the pioneering nature of the project.

Kollmorgen, a key partner in the project, supplied system software and vehicle hardware for fleet management, routing, and navigation solutions. Mikael Ekman, Key Account Manager at Kollmorgen, emphasized the versatility of Kollmorgen NDC Solutions, enabling automation across various vehicle types and navigation methods. Mikael noted the successful transition from manual to automated operations, with emphasis on the meticulous change management and stakeholder involvement achieved by DB Schenker Land in Borås.

Automotive Manufacturing Logistics

Automotive manufacturing demands precision. AGVs ensure reliable material flow, reduce downtime, and improve efficiency—supporting just‑in‑time production while increasing accuracy and overall performance.
Learn More

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.

CVC700HW Datasheet >

The CVC700 vehicle controller is a first step toward a modular AGV system. It offers increased processing power and enhanced communication, using the same successful form factor and IP65 housing as the CVC600