Skip to main content
press_release | Advanced AGV Cleaning High-Risk Zones to Recover Critical Metals in Gigafactories |
|
minute read

Advanced AGV Cleaning High-Risk Zones to Recover Critical Metals in Gigafactories

As gigafactories and recycling plants scale to meet rising demands, the need for innovative solutions that address both safety and efficiency continues to grow. DREV and Kollmorgen – Autonomous Mobile Solutions (AMS) are proud to announce their partnership and joint efforts to develop a groundbreaking Automated Guided Vehicle (AGV) with integrated contamination control technology. Designed to operate in large, highly restricted and hazardous environments, this AGV aims to ensure the safety of workers by operating where humans should not, while at the same time recovering valuable raw materials that would otherwise be discarded as dust.

“By combining DREV's expertise in contamination control with Kollmorgen's industry-leading AGV systems, we're driving innovation in the battery industry, delivering solutions that safeguard people and the environment.” – Thomas Tingelöf, CTO & Co-Founder, DREV.

Meeting the Challenges of Restrictive Industrial Environments

Modern industrial facilities face a growing challenge of maintaining productivity and ensuring safety in hazardous and highly restrictive areas where human access is limited or unsafe. Gigafactories, in particular, handle valuable and scarce raw materials that can be difficult to recover while also ensuring worker safety in these high-risk environments.

“This innovation addresses a critical gap in the industry and will be vital for maintaining safety and sustainability in future operations.” – Fernando Sosa, Senior Director of Facility & EPC, NOVO.

A High-Tech Solution for Efficiency and Safety

The collaboration between DREV and Kollmorgen AMS underscores a shared commitment to delivering practical, high-tech solutions for modern industrial operations. By prioritizing both safety and resource recovery, this AGV is set to redefine how gigafactories and recycling facilities handle complex logistics in high-risk environments.

“The DREV Vault-Autonomous System represents a breakthrough solution that combines Kollmorgen’s robust, proven and scalable technology for vehicle automation with DREV’s innovations that focus on employee safety in a fast growing and demanding industry. With advanced fleet management capabilities, operators can maintain high levels of productivity while minimizing risks to personnel.” – Johan Lundblad, General Manager, Kollmorgen AMS.

 

About Kollmorgen – Autonomous Mobile Solutions

NDC Solutions by Kollmorgen, a Regal Rexnord brand, is an industry leading platform utilized by top vehicle builders to create driverless logistics automation solutions. The platform consists of both software to manage fleets and route vehicles efficiently, and hardware for navigation and control. With Kollmorgen’s NDC Solutions you may automate virtually any type of vehicle or mobile robot and integrate it into any type of material handling application, in any industry, worldwide. Learn more: www.kollmorgen.com/agv

About Drev

DREV revolutionizes industrial cleanliness with cutting-edge contamination control technology designed for the world's most advanced manufacturing facilities. Bridging the gap between modern factory technology and traditional cleaning methods, DREV's innovative solutions eliminate water and harsh chemicals, while transforming waste into valuable resources. Specifically tailored for advanced industries with high-stakes environments and quality control standards, DREV's technology enhances material recovery and promotes a closed-loop system, enabling the recycling of precious materials such as lithium, nickel, and cobalt. Learn more: https://drev.tech

Automotive Manufacturing Logistics

Automotive manufacturing demands precision. AGVs ensure reliable material flow, reduce downtime, and improve efficiency—supporting just‑in‑time production while increasing accuracy and overall performance.
Learn More

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.