Skip to main content
press_release | Is This the End of Manual Pallet Adjustments in Logistics? |
|
minute read

Kollmorgen + ifm

Bridging the Gap Between Manual Handling and Smart Automation

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on precise location data to pick up and transport loads. These misalignments can lead to failed docking attempts, delays, and reduced productivity.

To solve this, Kollmorgen launched NDC Flex in 2023, which is a flexible solution designed to bridge the gap between AGVs and AMRs. One of its key capabilities, Dynamic Load Docking, enables vehicles to detect and align with the actual position of pallet loads in real time, regardless of placement accuracy.

Technology That Aligns: A Strategic Collaboration with ifm

After evaluating alternative solutions, Kollmorgen identified ifm’s 3D camera technology as the optimal choice—meeting the technical requirements and aligning with Kollmorgen’s strategic vision for future innovations. This led to a focused collaboration to integrate ifm’s pick solution into the Dynamic Load Docking capability.

As part of this effort, Kollmorgen added support for camera integration within the system software. This enhancement enables vehicles to handle off-coordinate pallet placements with precision, ensuring smoother and more reliable handovers between human and automated operations.

Collaborative Engineering in Action

The collaboration between Kollmorgen and ifm began with a series of productive technical meetings and hands-on testing sessions. ifm provided access to their equipment, and their application engineer worked closely with Kollmorgen to integrate the camera into the system. Thanks to strong teamwork and open communication, the team quickly aligned on the necessary steps to incorporate the technology into the system software.

Today, the camera communicates directly with the truck through its video-process unit, enabling dynamic route adjustments based on real-time data—bringing smarter automation to your operations.

Smarter Docking, Seamless Operations—Now Available

By adding this capability, you won’t compromise on high throughput or operational efficiency. Thanks to Kollmorgen’s extensive global partner network, this functionality is readily available to support smarter, more resilient automation—wherever your operations are.

See the Collaboration in Action Contact Kollmorgen

Automotive Manufacturing Logistics

Automotive manufacturing demands precision. AGVs ensure reliable material flow, reduce downtime, and improve efficiency—supporting just‑in‑time production while increasing accuracy and overall performance.
Learn More

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.

CVC700HW Datasheet >

The CVC700 vehicle controller is a first step toward a modular AGV system. It offers increased processing power and enhanced communication, using the same successful form factor and IP65 housing as the CVC600