AKD2G DS402 and Manufacturer Specific Torque and Current Setpoint and FeedbackFor AKD1G ECAT users the objects 2071h and 2077h do not exist. See the following app note for equivalents with the AKD2G ECAT drive. |
Will Gaffga |
English | |
S-Curve Corner Transition – Design and CalculationsThe reason the S-Curve Corner Transition was designed was due to the existing Corner Distance Transition having a discontinuity in the acceleration vector when entering the circular arc of the transition. If the axes group is travelling in a line at constant speed, the acceleration vector is zero… | Jeanie |
English | |
CNC PPC - Registradores especiais do CNCLista de registradores especiais do CNC para acessar dados em tempo real, status do CNC e comandos. |
Will Gaffga |
Portuguese, Brazil | |
Retrofit KAS EtherCAT Backups with AKD2G FirmwareThe AKD2G drives with firmware versions 02-12-00-001 (and later) do not support downgrading the firmware to the versions 02-12-00-000 (or earlier). The KAS EtherCAT backups created using AKD2G firmware 02-12-00-000 (or earlier) are not capable of restoring the drive’s configuration once any AKD2G… | Jeanie |
English | |
AKD2G EtherCAT W7011 Warning and F7011 Fault Synchronization Error SupportThis article provides details related to cause and remedy of the W7011 warning and F7011 Fault in the AKD2G EtherCAT drive. |
toddevans01 |
English | |
Convert AKD-B Parameter File to AKD-PInstructions to convert a saved AKD-B parameter file into an AKD-P file to load into an AKD-P drive. | kdn-adm |
English | |
Using Siemens PD_TEL9_DrivePos with Telegram 9 for Positioning with AKD2G Profinet RTThis document provides test results when using Siemens PD_TEL9_DrivePos function block with AKD2G Profinet Telegram 9 |
Will Gaffga |
English | |
KAS v4.01 Software is now available!! KAS v4.01 Software is now available!! |
dusty.schafer |
English | |
AKD and AKD2G Resolver Excitation Output Voltage Specification AKD and AKD2G Resolver Excitation Output Voltage Specification |
Will Gaffga |
English |
Don't know if you need a servo or stepper?
Have You Considered a Frameless Motor?
Read MoreEngineer the Exceptional
Learn More