AKD Modbus TCP Landing Page
AKD Modbus TCP Landing Page
Note: This Landing Page primarily applies to the AKD-B, P, or T drives. There are other application notes and guides for KAS with PCMM and PDMM controllers on the Kollmorgen Developer Network. See those articles for details that apply to that platform.
Overview and Specifications
Overview
The Modbus protocol is a communications protocol that is based on a client-server architecture. It was created in 1979. In the industry, Modbus has developed into a de facto standard since it is an open protocol.
Modbus allows connecting a server and several clients, usually via Ethernet. Three different operating modes are differentiated for data transmission: Modbus ASCII, RTU and TCP.
Each bus participant must have a unique address. In this case, the address 0 is reserved for a broadcast. Each participant may send messages via the bus.
Kollmorgen AKD Drive offers the TCP mode Modbus. TCP/IP packets are used to transmit the data. The TCP port 502 is reserved for Modbus TCP.
Note: The AKD-P-NxPN (Profinet) drive is the only AKD model in the family that does not support Modbus TCP communications.
-Related Articles
Modbus TCP Overview As It Relates To The AKD Drive
AKD Telnet And Modbus TCP Communications
Modbus TCP With AKD Compared To Fieldbuses
-Specifications and Update Rate
AKD X11 Service Port Specification
Modbus Holding Register Refresh Rate
_____________________________________________________________________________________________
Training
AKD Modbus Training Powerpoint Presentation
______________________________________________________________________________________________
Application Notes
-Motion Tasking
AKD Modbus Motion Tasking And Control
AKD Motion Tasking Over Modbus TCP
Saving The Motion Task Over Modbus
Understanding MT.LOAD and MT.SET
How To Configure Motion Task Using Modbus 64 Bit Parameters To 32 Bit Mapping
-Jogging
-Fault Reading/Diagnostics
How To Read AKD Fault Indication Over Modbus TCP
-Dynamic Mapping
Dynamic Mapping With AKD Modbus TCP
-Special Registers
-Troubleshooting
AKD Modbus Addressing And Troubleshooting
AKD Modbus MSG.LOG and MSG.DUMP
-AKD BASIC
User Units In The AKD BASIC Drive
AKD BASIC Position Move Using Modbus
AKI HMI to AKD BASIC Decimal Data Entry Example
AKD BASIC Program Variables Access Over Modbus TCP Quick Start Part 1: Modbus Poll
Single Precision Floating Point Decimal for AKD Basic float variables
-AKD with 3rd Party Modbus Masters ( i.e. PLCs, HMI, etc. )
Exor Panel to AKD Via Modbus TCP Communication
Siemens S7-1200 and S7-1500 to AKD Drive using Modbus TCP
Trio Motion Controller Modbus TCP Communications to AKD1G
Using Maple Systems EZWare Plus for Modbus TCP to AKD1G
Home >
Knowledge Base >
FAQs >
Downloads >