When changing the frequency of the sinusoidal profile, you may notice noise and resonance at different frequency values. There are several possible causes.EMI - Make sure all your cables are properly shielded and ground the shields. Make sure…
New Features
Next Generation Controller Software
Compatible with PCMM/PDMM (1st Generation Controllers)
64-bit Runtime (2nd Generation Controllers)
AKD2G Modular Device Profile (MDP) I/O
MDP IO support for model variants
New…
This article discusses AKD EtherCAT scaling for velocity, acceleration, and deceleration commands and actual velocity. For the position modes, FBUS.PARAM05 applies to position scaling and the scaling for velocity, acceleration, and…
The AKD drive supports flexible EtherCAT PDO mapping. The 4 available flexible RxPDO’s (PDO data for receive direction, commands from master to drive) are mapped using objects 1600h, 1601h, 1602h, and 1603h. Each one of these RxPDOs is…
PN.ACCSCALING sets the scaling factor for acceleration rates related to PROFINET motion commands.
The AKD PROFINET manual states that it applies to Jog Acc (PNU 1006), Jog Dec (PNU 1007), DRV_ACC (Telegram Signal 108), and DRV_DEC…
When migrating from AKD EtherCAT IP mode (Interpolated Position) to AKD2G EtherCAT CSP mode (Cyclic Synchronous Position), the only thing that needs to be changed is the target position object (change from 60C1h sub1 to 607Ah).
IP mode is supposed…