Skip to main content
blog | What are the basic elements of a servo system? |
|
2 minute read

What are the basic elements of a servo system

In its basic form, a servo system consists of an actuator (the muscle), a control device (the brain), and a feedback element (the senses). In the automation world, while the muscle can be a variety of mechanisms, it is most likely represented by a servo motor. The brain can also be represented by a variety of elements but is typically a motion controller or servo drive. The sense provides feedback information to the brain through a current sensor and/or an encoder, resolver, or even a vision system.

When the control device sends a signal to the actuator to move to a specific position, the actuator starts to move, and the feedback device signals back to the controller where and how fast the actuator is moving. The controller then reviews the feedback and determines if the motor has reached the commanded position. If not, the control device will continue to signal the actuator to move until it receives a signal from the feedback device that the motor has reached the desired position.

The servo system operates much like the processes of the human body - a remarkable multi axis motion system of hundreds of muscles, multiple feedback devices, and a control system that makes swift adjustments. As an example, a baseball player steps up to the plate to bat and the brain analyzes the current situation, the number of players on base, the current number of outs, the position of the defense. The batter glances toward the third base coach and receives the signal to hit the ball (the image passes from the eyes to the brain). As the pitcher throws the ball, the batter anticipates the pitch, and contemplates where the ball will cross the plate. As the pitcher releases the ball, the batter’s eyes send information to the brain, the brain analyzes the ball’s flight, makes split second decisions, sends signals to multiple muscles, and coordinates the swing of the bat to precisely hit the ball. If the batter misses the ball, the brain analyzes the error to adjust for the next pitch. The human body, like a servo system, works in a coordinated dance of precision motion. The modern industrial servo system has advanced significantly and now includes complex controllers with multiple feedback devices and fast processors that make nanosecond decisions to perform the desired motion. A breakdown of a typical industrial servo system includes:

Kollmorgen Automation System - Component diagram
  • Servo motor – the muscle of the system, available in a variety of technologies including brush or brushless, housed or frameless, and linear or rotary. The motor produces the torque required to accelerate and move the load.
  • Servo drive – this can be either the brain of the system or a portion of the brain. Simple servo drives may control torque and/or speed, while higher level servo drives offer additional features and can be configured as a positioner with programming capabilities. A drive or controller, matched to the servo motor, controls the voltage and current the motor receives.
  • Servo controller – the brain of the system, utilizes a programming environment to allow a variety of options for machine control, operation of inputs and outputs, and is interconnected with a type of graphical user interface. Servo controllers can be standalone or integrated with servo drives.
  • Feedback – the senses of the system is typically integrated into the servo motor. The feedback element can consist of an encoder, resolver, linear feedback device, tachometer, etc. Sophisticated control systems may include more advanced forms of feedback such as a vision system.
  • Cabling – The servo system is interconnected so the feedback, communication, and power feedback cabling becomes the nervous system that connects the brain, muscles, and senses together.

Selection of the right set of components for a servo system demands a careful analysis of the system performance requirements. The amount of “muscle” required will determine the size of the servo motor, which in turn affects the selection of the servo drive. The precision of the application plays a role in feedback selection, specifically for the type and resolution of the feedback device. The amount of coordination between other devices in the system, along with the response required, will determine the level of controller required.

Putting this all together can be a considerable task. Working with motion control experts like Kollmorgen makes selecting a servo system easier and faster, resulting in an optimal system for the application.

Consult an Expert

AKME Series Servo Motors

AKME Series is built on the AKM platform and designed for use in Zone 2 and Zone 22 environments with ATEX and IECEx global certification.
Learn More

AKMA Servo Motors

The lightweight AKMA servo motor is designed for harsh environments like food and beverage processing, and delivers performance and reliability.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Automatic Pick and Place machine installing components on circuit board

How mechatronics design improves motion system performance >

Discover how mechatronics design boosts motion system performance by integrating servo systems and control for faster commissioning and integrated motion.
Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple

Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple >

Introducing Kollmorgen’s AKME servo motors—ATEX/IECEx certified and engineered for compact, versatile performance in hazardous environments where choices have been limited—until now.
Introducing the latest update to SafeMotion monitor firmware - SMM 3

Kollmorgen advances linear motor safety and performance with SafeMotion Monitor firmware upgrade >

The latest SafeMotion Monitor™ firmware (SMM 3.0) expands functional safety for linear motors with EnDat 2.2 safe feedback support and SIL 3 compliance.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK
Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español)

Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español) >

Descubre cómo Kollmorgen Essentials ofrece control de movimiento de alta precisión y fiabilidad comprobada, ahora más rápido de configurar, más fácil de integrar y más rentable de escalar.
Español
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.