Skip to main content
press_release | Kollmorgen advances linear motor safety and performance with SafeMotion Monitor firmware upgrade |
|
minute read

Introducing the latest update to SafeMotion monitor firmware - SMM 3

RADFORD, VA. — Kollmorgen Corporation, a global leader in motion control systems, released the next update for the SafeMotion™ Monitor (SMM) firmware: SMM 3.0. This upgrade expands functional safety support for linear motors and linear axes, helping machine builders implement functional safety in applications ranging from semiconductor manufacturing to battery production and industrial automation that require safety.

Integrated into AKD2G servo drives and the Kollmorgen 2G Motion System, SMM 3.0 continues to work with all motors that feature any HIPERFACE DSL® rotary-safe feedback system. It also allows the AKD2G drive to now support EnDat 2.2 safe feedback systems to better serve the growing demand for high-performance safety solutions in precision motion control.

​​​Performance Meets Safety

The EnDat 2.2 safe protocol, now supported by ADK2G drives and 2G Motion System, delivers dual independent positioning for robust error detection, high-speed serial data transmission for fast cycle times, integrated diagnostics with comprehensive monitoring, and flexible encoder support for incremental and absolute feedback drives.

“Linear motors deliver unmatched performance, but implementing functional safety can be challenging,” says Chris Cooper, Product Management Senior Director at Kollmorgen. “The newest update for the SafeMotion™ Monitor (SMM) firmware solves this by bringing EnDat 2.2 safe feedback support to our platform, giving machine builders a complete safety solution that doesn’t sacrifice the speed and precision of linear motors.”

Kollmorgen’s AKM2G and AKMA servo motors also include an EnDat 2.2 safe feedback option, offering even higher performance and accuracy than HIPERFACE DSL for axes where functional safety is required. When combined, machine builders get a complete, integrated motion solution for safety-related applications.

SIL 3 Capability

SMM 3.0 enables complete motion systems to achieve Safety Integrity Level 3 (SIL 3) certification. While the AKD2G drive has maintained SIL 3 certification since launch, the addition of EnDat 2.2 safe feedback support now provides a complete, matched solution capable of meeting this rigorous standard. This is especially important where operators face frequent high-risk scenarios, such as stage lifting systems and heavy material handling equipment. Furthermore, the SIL 3 capability helps future-proof systems so they can scale as safety requirements evolve.

To learn more about the updated safety option and all of our functional safety solutions, visit https://www.kollmorgen.com/en-us/solutions/industry/safety.

 

About Kollmorgen

Kollmorgen Corporation, a Regal Rexnord™ brand, has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, AGV control solutions and automation control platforms. We deliver breakthrough solutions that combine exceptional performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

The following are believed to be the trademark and/or trade names of their respective owners and are not owned or controlled by Regal Rexnord Corporation. EnDat: Dr. Johannes Heidenhain GmbH; HIPERFACE DSL: SICK AG.

Regal Rexnord is a trademark of Regal Rexnord Corporation.

©2026 Kollmorgen Corporation, All Rights Reserved.

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor phase-sequencing issues.

Learn More

Safety

Learn more about Kollmorgen SafeMotion™ control functions, which are 100% drive-resident and eliminate the need for external functional safety solutions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK
Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español)

Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español) >

Descubre cómo Kollmorgen Essentials ofrece control de movimiento de alta precisión y fiabilidad comprobada, ahora más rápido de configurar, más fácil de integrar y más rentable de escalar.
Español
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments >

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor…
Kollmorgen expands functional safety support with SafeMotion™ Monitor upgrade

Kollmorgen expands functional safety support with SafeMotion™ Monitor upgrade  >

The latest update to SafeMotion™ Monitor (SMM) firmware — SMM2.0 — enables use with a wider range of encoders for new high-performance applications.