Skip to main content
blog | Kollmorgen Is on the Perseverance Rover—And Extreme Environments Everywhere |
|
2 minute read
Kollmorgen Is on the Perseverance Rover—And Extreme Environments Everywhere

From the surface of Mars to the depths of the ocean, from the core of the earth to the core of the human body, Kollmorgen motion systems take on the most extreme environments.

For the vast majority of applications, motors perform in everyday environmental conditions. And while a motor failure may be inconvenient, or even lead to expensive downtime, it rarely causes a catastrophic and irrecoverable failure of the application. Then again, there are specialized, high-stakes applications where the environment is extreme and failure is not an option. Space exploration is the most striking example.

How can you dissipate heat generated by instruments, control electronics and power sources in the vacuum of space? On the flip side of the coin, how can you ensure reliable operation of motion systems when ambient temperatures approach absolute zero? How can you prevent vacuum-accelerated outgassing of materials that could contaminate sensitive components and experiments? How can you ensure that materials withstand the intense radiation from space as well as from the space vehicle’s own plutonium energy source?

Six Decades and Hundreds of Motors in Space

The Perseverance Rover has just begun its mission of at least one Martian year (687 Earth days), and hopefully much longer, exploring the surface of the red planet. It represents possibly the most advanced feat of engineering ever attempted—and it’s just the latest in a long history of remarkable space journeys that Kollmorgen has helped make possible.

Kollmorgen has been supplying motors for NASA programs since the Gemini missions of the mid 1960s and continuing through the Apollo moon landings, the Skylab space station, the GPS satellites that are so critical to everyday life and commerce, Titan rocket guidance systems, the Space Shuttle reusable low-Earth orbiter, and many more. And Kollmorgen motors have been on Mars programs beginning with Viking 1—the first lander to succeed in its mission—through the Spirit, Opportunity and Curiosity rovers, and now the remarkable Perseverance. Over the course of nearly six decades, we have put hundreds of motors into space.

The Heart of the System

Engineering a project like Perseverance is truly a team effort, and we’re proud to be part of the team. Among our many contributions to NASA engineering is a co-engineered RBE Series direct drive frameless motor that drives Perseverance’s critical thermal-management pump, which cools all electronics and instruments onboard the rover. NASA engineers fondly refer to it as “the heart of the system.”

RBE Series motors are ideal for this purpose as the frameless configuration can be integrated directly into the application, using the same bearings to support both the load and the rotor to minimize volume, weight and complexity. The co-engineered RBE design also incorporates materials that can withstand the rigors of space. And a special modification allows for installation of a unique liquid cooling system for the motor itself—designed for reliable, long-term performance under the most extreme conditions.

RBE

We are currently working directly with NASA’s Jet Propulsion Laboratory to optimize this co-engineered RBE motor for long-term use on the Europa Clipper Orbiter, scheduled to launch in 2024 and arrive in Jupiter orbit in 2030, where it will map out Europa and other Jovian moons. Our motor will control the pump on the Orbiter’s critical thermal-management system, and is expected to operate throughout a 12-year mission.

What’s Your Extreme Environment?

Supplying motors for space missions may sound exotic, but designing and building motion systems for extreme environments is business as usual for Kollmorgen. And think about it. Extreme environments, where failure is not an option, aren’t just found in outer space or on the surface of Mars. They’re above, below and all around us.

  • Kollmorgen motion systems help control flight in everything from commercial aircraft to hypersonic missiles.
  • They’re on food and beverage production lines, with hygienic designs built to endure the daily washdowns that can quickly destroy lesser motors.
  • They’re in medical equipment, from surgical robots to high-resolution CT scanners to implantable devices—such as left ventricular assist devices that literally help keep people alive, healthier, longer.
  • They’re deep beneath the Earth’s crust, enduring the extreme temperatures, pressures, corrosives and hazardous atmospheres encountered in oil and gas production.
  • They drive and control the robots used to safely remove and replace fuel rods in nuclear power plants.
  • Kollmorgen motion systems even help propel and guide underwater vehicles, from the Jason Jr. that explored the Titanic wreck to vehicles designed for the deepest depths that humans and mechanics can go.

And those are just a few of the unclassified programs that we’re allowed to talk about. Don’t see your application on the list? That’s not the point. Kollmorgen has the technology, product range, co-engineering know-how, broad industry expertise and commitment to help you solve practically any motion challenge, no matter what it may be.

Your mission doesn’t need to be searching for evidence of extraterrestrial life. If you’re searching for precise, reliable, perfect-fit motion that you can count on to perform under any conditions, we’re ready to help you engineer the exceptional.

So let’s get started. Consult a Motion Expert

Consult an Expert

Direct Drive Linear Motors

Using Kollmorgen DDL direct drive linear motors, your machine can be simpler, faster, more precise and reliable. Pair your ironless, low profile or ironcore linear motor with an AKD or AKD2G servo drive for industry-leading power density.
Learn More

Frameless Motors

Discover Kollmorgen's frameless motor range, designed for easy integration into your application, enhancing performance, efficiency and reliable motion solutions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Space satellite

Engineering Motion Systems for Space: A Guide to Reliability, Scalability and Mission Success >

Move from terrestrial prototypes to mission success with a practical guide on evaluating space-ready motors and engineering spacecraft motion control.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
RBE Series Motors Selection Guide

RBE Series Motors Catalog >

The RBE series brushless motors provide a wide range of flexible motor solutions for frameless DDR (Direct Drive Rotary) motor applications. These motors come in either housed (RBEH) or frameless (RBE) mechanical configurations.
Advanced Motion Solutions for Next-Gen Space Missions

Advanced Motion Solutions for Next-Gen Space Missions >

Space exploration is undergoing a new renaissance, with thousands of new satellites planned. Motion systems that meet both the extreme demands of space and the realities of the marketplace will be key to winning the space race. This webinar will…
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…
High-Voltage Direct Drive Linear Motors Take Machine Tool Performance to New Heights

High-Voltage Direct Drive Linear Motors Take Machine Tool Performance to New Heights >

IC Ironcore DDL linear motors and AKD servo drives delivered 65% greater positioning accuracy and 15% higher productivity for this double-faced grinding machine.