Skip to main content
Success Story | 2 minute read

Compact robotic actuator

Designing modular robotic platforms is a balancing act. A single actuator needs to perform across multiple configurations including robotic arms, legs and mobile bases. However, each configuration has different torque, speed and environmental requirements which can often lead to compromises that limit performance at the joint system level.

HEBI Robotics is on a mission to make robots more accessible by simplifying how they are designed and assembled with standardized building blocks. For over a decade, their modular approach has been applied across a wide range of challenging applications—from snake robots and hexapod walkers to robotic arms and mobile bases for pipeline inspection, Non-Destructive Testing (NDT), maintenance and more.

As HEBI expands further into industrial settings, a new customer project reinforced the opportunity to expand their actuator lineup to better meet challenging or hazardous workspace needs without any performance tradeoffs.

Challenge

HEBI’s customer project required a robotic system capable of traversing complex, confined spaces and positioning inspection probes and other heavy tooling with a high degree of accuracy and repeatability. The environment was highly variable and closer to real-world industrial conditions like those found in Oil & Gas, infrastructure or other rugged settings.

Rather than relying on HEBI’s established series of high-ratio elastic actuators that use spur‑gear reductions, the project required high torque density actuators and more accurate motion across multiple degrees of freedom—without increasing size or sacrificing architectural flexibility.

This meant rethinking how the motor itself was integrated into the actuator. 

“TBM2G’s compact size and high torque allow us to develop smoother, faster, and more precise next‑generation robotic joints. We love this motor.”
 — Dave Rollinson, Chief Technology Officer, HEBI Robotics

Solution

To achieve the required shift in performance, HEBI focused on integrating the motor directly into the compact actuator design. This approach led to the selection of Kollmorgen’s TBM™2G frameless motors as the foundation for the new H-Series Actuator®.

The frameless motor architecture allowed HEBI to optimize torque density, thermal performance and modularity at the joint level. By integrating the stator and rotor directly into the high torque density actuator, the H-Series delivers smoother motion and faster dynamic movement with higher accuracy—and without adding to the actuator’s overall size.

The teams from Kollmorgen and HEBI collaborated throughout motor selection and integration to optimize motor configuration for the application. This collaboration helped streamline development and ensure the compact actuator design met performance targets for both the H-Series line and the customer project at hand. 

10x more torque without increasing size of existing actuators

Results

The H-Series actuator delivered the performance gains and precision required for the confined-space inspection project. The system was able to position heavy tooling accurately while operating in tight mechanical constraints, exceeding specifications and motion expectations under real operating conditions. 

By pairing the TBM2G frameless motor with strain wave gearing, the H-Series achieved zero backlash motion and up to 10 times more torque than their existing actuator line. This increase in torque density enabled HEBI to expand the capabilities of the entire joint system without increasing actuator size. The actuator’s compact, sealed design—rated IP65—supports operation in challenging, rugged environments.

Beyond just raw performance, the H-Series Actuator simplifies manufacturing and assembly. Moving from a more complex actuator design to a streamlined, frameless motor-based approach improves ease of manufacturability and creates a clearer path to scaling production. The high torque-to-size ratio of the motor also created space within the actuator for embedded electronics, enabling smarter joints without increasing size.

Kollmorgen’s responsiveness and engineer-to-engineer collaboration played a key role throughout the selection, design and integration process. Close technical support and U.S.-based manufacturing helped HEBI move efficiently through development to deployment.

All in all, the results position the H-Series Actuator as a powerful expansion in HEBI’s revolutionary modular robotic platform with Kollmorgen’s frameless motor at the core. Together, the combination is helping build the next phase of how HEBI shapes the way our world works.

Download as PDF

Incorporating Frameless Motors Into an Environmentally Resilient Design

Daily washdowns, deep-sea submersion, high radiation, high vacuum, hazardous atmospheres: When a housed servo motor can’t provide the protection you need in a compact form factor, consider embedding a frameless servo motor. Read this white paper to learn how.

Learn More

Achieving Ultimate Motion Precision Using Frameless Servo Motors

Frameless motors aren’t just for robotic joints. Compact actuators, sensor system gimbals, submersible propulsion systems and other applications benefit from direct drive precision and compact design. Learn how to directly embed a frameless motor in your mechanism.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
Designing Field Robots for Harsh and Unpredictable Environments

Designing Field Robots for Harsh and Unpredictable Environments >

This session explores how innovative technologies from Kollmorgen and Regal Rexnord’s broad portfolio of motion control technologies can help engineers meet the rigorous demands of field robotics.
Motion Control Principles for Scalable Humanoid Robotics

Motion Control Principles for Scalable Humanoid Robotics >

As humanoid robotics gain momentum across industries—from logistics and manufacturing to healthcare and public safety—the demand for precise, efficient, and scalable motion control solutions is accelerating. Engineers face complex challenges in…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…