Skip to main content
blog | Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability |
|
2 minute read

Minesweeping UGV

Designing small tracked Unmanned Ground Vehicles (UGVs) for minesweeping is a unique engineering challenge. These robots must be compact enough to navigate rugged terrain, powerful enough to handle heavy-duty detection equipment, and reliable under harsh environmental conditions.

Why Frameless Motors for Minesweeping UGVs?

Frameless motors are ideal for defense and security robotics because they allow direct integration into the mechanical structure, reducing weight and allowing design engineers to reduce the footprint of their UGVs. For tracked UGVs, frameless motors can be embedded into drive systems or actuator assemblies, enabling a low-profile design that minimizes exposure to hazards while maximizing maneuverability.

Three Key Design Considerations:

1. Torque Density vs. Size

Tracked UGVs require high torque to overcome uneven terrain and obstacles while maintaining precise control for minesweeping operations. Frameless motors follow the D²L rule—torque increases with the square of diameter and linearly with length.

For compact UGVs, increasing diameter is often preferable to length, as longer motors complicate integration into low-profile chassis designs. However, larger diameters can limit space for sensors and electronics, creating a design footprint tradeoff.

Design Tip: Choose frameless motors optimized to deliver the required torque with short axial lengths. Compact designs simplify integration without sacrificing performance.

2. Velocity vs. Torque

Minesweeping UGVs need controlled speed for scanning accuracy, but they also require bursts of torque for climbing inclines or towing auxiliary equipment. Harmonic or planetary gearing can help balance these needs, but high gear ratios reduce speed.

Frameless motors capable of maintaining torque at higher RPMs are essential to avoid oversizing the motor and adding unnecessary weight. This is especially true when considering that these systems are usually operating at lower DC bus levels, typically 48 VDC.

Design Tip: Select motors with advanced winding technology that sustain torque across a broad speed range, reducing the need for oversized designs.

3. Temperature vs. Reliability

Operating in hot climates or under continuous load can push motor winding temperatures beyond safe limits. Excess heat degrades lubricants, sensors and electronics—critical components for minesweeping reliability. Motors optimized for lower thermal rise and equipped with integrated thermal sensors help prevent failures.

Design Tip: Look for frameless motors engineered to maintain performance across a wide range of winding temperatures, ensuring long-term durability of gearboxes and electronics.

Environmental and Safety Factors

Minesweeping robots often face dust, moisture, shock and vibration. Frameless motors allow the designer to provide the level of sealing integration to meet mission demands.

Recommended Motor Features for Minesweeping UGVs

  • Compact axial length with high torque density
  • Wide speed range with minimal torque drop-off
  • Integrated thermal and Hall sensors for feedback
  • Materials and design suitable for harsh environments
  • Compatibility with off-the-shelf gearing systems

The Right Choice for Your UGV

Frameless motors are not just a component—they define the agility, endurance and safety of minesweeping UGVs. By prioritizing torque density, thermal management and environmental resilience, designers can create robots that perform reliably in the most demanding conditions without compromising size or efficiency.

Kollmorgen’s TBM, TBM2G and KBM series exemplify how high torque meets compact, integration-friendly form factors. If you're designing tracked UGVs for minesweeping or other ground applications, learn how we can provide the mission-critical performance you demand. Our motion experts are here to help find the right balance of power, size, weight and reliability.

Consult an Expert

Frameless Motors

Discover Kollmorgen's frameless motor range, designed for easy integration into your application, enhancing performance, efficiency and reliable motion solutions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Driving Aerospace & Defense Innovation with Motion Technology >

Motion technology is the execution layer that turns AI and software into physical mission readiness. Explore how it drives aerospace and defense innovation at scale.
Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Space satellite

Engineering Motion Systems for Space: A Guide to Reliability, Scalability and Mission Success >

Move from terrestrial prototypes to mission success with a practical guide on evaluating space-ready motors and engineering spacecraft motion control.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Designing Motion Control for Turrets and Large Azimuth Drive Systems in Military Ground Vehicles

Designing Motion Control for Turrets and Large Azimuth Drive Systems in Military Ground Vehicles >

It’s important to distinguish between technology and topology when designing motion systems for large military ground vehicles. Topology is the high-level architecture of how those components are arranged and interact within your system.
Motion Design for Next-Generation Armored Fighting Vehicles

Motion Design for Next-Generation Armored Fighting Vehicles >

Learn what to consider when designing for next-gen armored fighting vehicles, from electromechanical motion architectures to mission-critical performance.
Technology vs. Topology: Designing Motion for Turrets and Large Azimuth Drive Systems

Technology vs. Topology: Designing Motion for Turrets and Large Azimuth Drive Systems >

Learn how to select the right motion system topology for your ground vehicle platform and go from concept to combat success with Kollmorgen.