Skip to main content

Advancing Exoskeleton Technology with Motor Compliance

Exoskeletons present a formidable engineering challenge, necessitating designs that are both lightweight and powerful; compact yet comfortable for the user. Regardless of the application, motion design and motor selection are make-or-break steps in the engineering process.

How can these choices help (or hinder) the ultimate performance, which must mimic the complex mechanics of the human body? Here we explore key considerations and insights.

Read the Blog

Advancing Exoskeleton Technology with Motor Compliance
Greater Comfort & Safe Mobility in Exoskeleton Design

Greater Comfort & Safe Mobility in Exoskeleton Design

As wearable devices, exoskeletons must be comfortable, reliable and safe — a tall order given their extremely complex mechanics. Engineers must consider three main criteria when designing exoskeletons for commercial viability: keeping temperatures low enough to enable humans to safely wear them; minimizing the risk of accidents and injuries; and ensuring optimal mobility for the user.

These requirements entail careful design — and the selection of a motor designed to work specifically with exoskeleton joints.

Read the Blog

Accelerating from Exoskeleton R&D to Full-rate Production

The exoskeleton market to date, has been built on smaller volumes and custom production. As the industry shifts — and exoskeletons become more common and viable for everything from medical rehabilitation and mobility to heavy load lifting — OEMs should be smart about the transition to efficient, high-volume production.

But moving to full-rate production presents a new set of challenges and considerations. Projects that seemed feasible during R&D and even LRIP can quickly become impossible at scale for a variety of reasons. How can OEMs foresee (and avoid) issues that may arise as they ramp up production?

Read the White Paper

Accelerating from Exoskeleton R&D to Full-rate Production
TBM Series Medium Image

TBM Series Frameless >

Our TBM series provides direct drive frameless motors designed to be directly embedded in the mechanical structure of your systems, minimizing weight, size and inertia without sacrificing performance.

Kollmorgen TBM2G Frameless Motor

TBM2G Series Frameless >

These next-generation frameless motors deliver high torque density for your most compact, lightest electromagnetic package, standard sizing for harmonic gearing, and scalable design to keep you on top of your global production needs.

Related Resources

Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Designing Field Robots for Harsh and Unpredictable Environments

Designing Field Robots for Harsh and Unpredictable Environments >

This session explores how innovative technologies from Kollmorgen and Regal Rexnord’s broad portfolio of motion control technologies can help engineers meet the rigorous demands of field robotics.
Motion Control Principles for Scalable Humanoid Robotics

Motion Control Principles for Scalable Humanoid Robotics >

As humanoid robotics gain momentum across industries—from logistics and manufacturing to healthcare and public safety—the demand for precise, efficient, and scalable motion control solutions is accelerating. Engineers face complex challenges in…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…
Exoskeletons at Scale

Exoskeletons at Scale: Accelerating the Transition from R&D to Full-rate Production >

The exoskeleton market is still in its infancy — but evolving quickly and ripe with opportunity. It’s a double-edged sword for OEMs who must identify the most impactful applications and crack the code on full-scale production, which presents a new…